How to run USB UVC ( USB video class)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to run USB UVC ( USB video class)

5,427 次查看
vongocson
Contributor III

hi everyone

I'm doing with Yocto with  imx6qsabresd-board. who are teach me how to way runing usb uvc in terminal ( tera teram)?

root@imx6qsabresd:~# lsmod
Module Size Used by
mxc_v4l2_capture 24976 0
ipu_bg_overlay_sdc 5246 1 mxc_v4l2_capture
ipu_still 2312 1 mxc_v4l2_capture
ipu_prp_enc 5864 1 mxc_v4l2_capture
ipu_csi_enc 3601 1 mxc_v4l2_capture
ipu_fg_overlay_sdc 6072 1 mxc_v4l2_capture
imx122_camera 8655 0
uvcvideo 71690 0
ov5640_camera_mipi_int 23218 0
v4l2_int_device 2913 3 ov5640_camera_mipi_int,imx122_camera,mxc_v4l2_capture
mxc_dcic 6544 0

Best regard!

2 回复数

3,614 次查看
igorpadykov
NXP Employee
NXP Employee

Hi vo

please check

Using a USB Camera with GStreamer 

UVC camera not detected on i.MX6 SABRE board 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,614 次查看
vongocson
Contributor III

how to do usb slave? 

because when i connect with my pc, it's can't auto connect driver in my pc. this problem i can't understand.

Best regard

0 项奖励
回复