Here we just used the framebuffer based embeded QT, no X11 support.
1. Install the Freescale LTIB BSP, for example “L2.6.35_11.05.01_ER_source.tar.gz”
2. Goto ltib folder build the BSP for iMX board:
$ ./ltib –selectype
(1) Select imx5x platform and min profile:
(2) Save and goto next page, select the board for example “mx50_rdp”.
(3) In same page, goto “Target Image Generation”, and select “ext2.gz ramdisk” image for SD boot and save.
(4) Goto “Package List ” and select the “Tslib” to enable touch panel or QT, save.
(5) Save and exit, LTIB will start to build the image.
(6) The rootfs will be built out at ltib folder “rootfs”.
3. Get the “tslib” source code from LTIB: “$ ./ltib –p tslib -m prep”; the tslib source code can be found at “ltib/rpm/BUILD/tslib-1.0”
4. Set the CROSS_COMPILE for both tslib and QT compiling.
In Ubuntu, the LTIB cross compiler will be installed to “/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0”.
Edit “~/.bashrc”, and add the followed line, then logout and login again:
export PATH=/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/:$PATH
5. Build the tslib
$ cd ~/tslib-1.0
$ ./autogen.sh
$ echo "ac_cv_func_malloc_0_nonnull=yes" >arm-linux.cache
$ ./configure --host=arm-linux --cache-file=arm-linux.cache -prefix=/home/ubuntu123/tslib
$ make
$ make install
Now tslib head files and lib will be at folder “home/ubuntu123/tslib/”.
6. Build the QT, the last QT source code can be downloaded from “http://get.qt.nokia.com/qt/source/qt-everywhere-opensource-src-4.7.3.tar.gz”.
$ cd ~
$ tar -zxvf qt-everywhere-opensource-src-4.7.3.tar.gz
$ cd qt-everywhere-opensource-src-4.7.3
Edit the file “mkspecs/qws/linux-arm-gnueabi-g++/qmake.conf”, and add the line “QMAKE_LFLAGS += -Wl,-rpath-link=/home/ubuntu123/tslib/lib”.
$ ./configure -embedded arm -xplatform qws/linux-arm-gnueabi-g++ -prefix ~/qt_demo -hostprefix ~/qt_target -opensource -qt-mouse-tslib -I ~/tslib/include -L ~/tslib/lib -confirm-license
$ make
$ make install
Then the built out QT libs can be found at “/home/ubuntu123/qt_target”.
7. Prepare the rootfs
(1) Copy “/home/ubuntu123/qt_target/*” to “ltib/rootfs/qt” folder; copy “/home/ubuntu123/qt_demo/*” to “ltib/rootfs/qt”.
(2) Edit the file “ltib/rootfs/etc/profile”, and add the followed lines:
export QTDIR=/qt
export QPEDIR=/qt
export PATH=$QTDIR/bin:$PATH
export TSLIB_ROOT=/usr
export TSLIB_CONSOLEDEVICE=none
export TSLIB_FBDEVICE=/dev/fb0
export TSLIB_TSDEVICE=/dev/input/ts0
export TSLIB_PLUGINDIR=$TSLIB_ROOT/lib/ts
export TSLIB_CONFFILE=$TSLIB_ROOT/etc/ts.conf
export TSLIB_CALIBFILE=/etc/pointercal
export QWS_MOUSE_PROTO=Tslib:/dev/input/ts0
export QWS_DISPLAY=LinuxFb:/dev/fb0
export set QT_QWS_FONTDIR=$QTDIR/lib/fonts/
export LD_LIBRARY_PATH=$TSLIB_ROOT/lib:$QTDIR/lib:/usr/local/lib:$LD_LIBRARY_PATH
(3) “$ cd ~/ltib/rootfs”; “$ tar -jcvf ../rootfs.tar.bz2 .”; now the rootfs.tar.bz2 can be burned to iMX board with MFGTool.
8. Run the QT demo
After the board booted up, we can run “$ ts_calibrate” to calibrate the touch panel; use the followed commands to run the QT demos.
$ cd /qt/demos/mainwindow
$ ./mainwindow -qws