How to rotation 180 degree display in the android 4.3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to rotation 180 degree display in the android 4.3

3,055 次查看
juan_tang
Contributor III

BSP:android 4.3

EVK:MCIMX6Q-SDP

Need support: I changed the following line in the init.rc:

setprop ro.sf.hwrotation 180

But did not works.

标签 (2)
0 项奖励
回复
2 回复数

1,569 次查看
kobusgoosen
Contributor II

I had similar issues, but unfortunately I couldn't resolve this. The reason for this seems to be that the setprop ro.sf.hwrotation doesn't tell android which way the display is orientated, but what to accept as the default device rotation (like for a device without accelerometer).

(you can test this on an Android device in a rotatable app: if you rotate your phone left or right, it will rotate accordingly, but if you hold it upright and immediately hold it upside down, it will remain as is)

I fixed it on my system by changing the LVDS display invert X/Y pins so that it displays the other way around, and changed my touch driver to invert values... I'm sure there must be an easy way.



0 项奖励
回复

1,569 次查看
juan_tang
Contributor III

If I invert X/Y pin,just rotation 90 degree.I  want to rotation 180 degree. I just debug the IPU driver. I configured the rots parameter is "IPU_ROTATE_180 = 3" in the ipu_ch_param_set_rotation functionof the  ipu_common.c file.But the X axis is rotation, Y axis no change.I think is a problem of IPU drive.  

typedef enum {
/* Note the enum values correspond to BAM value */IPU_ROTATE_NONE = 0,
IPU_ROTATE_VERT_FLIP = 1,
IPU_ROTATE_HORIZ_FLIP = 2,
IPU_ROTATE_180 = 3,

IPU_ROTATE_90_RIGHT = 4,
IPU_ROTATE_90_RIGHT_VFLIP = 5,
IPU_ROTATE_90_RIGHT_HFLIP = 6,
IPU_ROTATE_90_LEFT = 7,
} ipu_rotate_mode_t;

0 项奖励
回复