Hi,
I am using Freescale IMX 6 series Quad Sabre board for Auto infotainment.
I am using the bsp package version "L3.0.35_12.09.01_GA_source" downloaded from freescale site.
When I checked the memory info ,I came to know that the board supports 256MB of RAM
I wanted to restrict the kernel space to 128MB and use the rest for some other purpose.
I tried giving the option "mem=128M" in the boot args.However the board was not booting after this change.
Please let me know the option to give so that I can restrict the memory available for kernel to 128MB.
Thanks in advance
Arun Krishna
已解决! 转到解答。
Hi Mr Yixing,Zhi Li,
I found out that the RAM supports 2GB(and not 256MB) of memory in total.It was showing this memory in 2 separate chunks(256MB and 1.7GB)...I did not see the second chunk when I listed down the available memory.
However we need to reserve atleast 512MB of memory for board to boot up and the graphics to come up.So when I use mem=512M the board gets booted up.
Thanks
Arun Krishna
Hi Mr Yixing,Zhi Li,
I found out that the RAM supports 2GB(and not 256MB) of memory in total.It was showing this memory in 2 separate chunks(256MB and 1.7GB)...I did not see the second chunk when I listed down the available memory.
However we need to reserve atleast 512MB of memory for board to boot up and the graphics to come up.So when I use mem=512M the board gets booted up.
Thanks
Arun Krishna