One customer uses one camera which can only support VGA(640*480), that is, their encoder obtains V4I2 data of VGA reolution from camera. If they use that V4I2 data to encode H.264 payload into other resolution, such as 4CIF(704*576), the encoded payload is bad.
Do you have any suggestion on this issue? I can send the encoder code to you. Thank you.
已解决! 转到解答。
Customer called the function v4l_capture_setup with the fixed width and height parameters(640, 480), after modified this part, it becomes normal.
MaxTsai Aug 25, 2013 10:24 PM (in response to imxcommunityscout)
hi I am not sure if this issue is resolved? Does the customer encode the data into H264 payload by software or by hardware?