How to resize PCIE window on IMX8QM?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to resize PCIE window on IMX8QM?

Jump to solution
2,782 Views
lmendes
Contributor III

 

I am trying to resize the PCIE windows (in file imx8qm-ss-hsio.dtsi), so that, PCIEA becomes larger with 256MB MEM window plus default IO window, while shortening PCIEB in order to release space for PCIEA, like so:

     pciea: pcie@0x5f000000 {
         reg = <0x5f000000 0x10000>, /* Controller reg */
               <0x70000000 0x80000>, /* PCI cfg space */
               <0x5f080000 0xf0000>; /* lpcg, csr, msic, gpio */
        reg-names = "dbi", "config", "hsio";
        ...
        ranges = <0x81000000 0 0x00000000 0x70080000 0 0x00010000 /* downstream I/O */
                  0x82000000 0 0x60000000 0x60000000 0 0x10000000>; /* non-prefetchable memory */
        ...
     

and PCIEB to:

     pcieb: pcie@0x5f010000 {
        reg = <0x5f010000 0x10000>, /* Controller reg */
              <0x7ff00000 0x80000>, /* PCI cfg space */
              <0x5f080000 0xf0000>; /* lpcg, csr, msic, gpio */
        reg-names = "dbi", "config", "hsio";
        ...
        ranges = <0x81000000 0 0x00000000 0x7ff80000 0 0x00010000 /* downstream I/O */
                0x82000000 0 0x71000000 0x71000000 0 0x0ef00000>; /* non-prefetchable memory */

But when I do this, the Linux kernel is not able to setup the windows and the WiFI card is not detected on PCIEB, nor any card on PCIEA.

Even if I simply modify PCIEB leaving PCIEA unchanged, is enough for the PCIEB window not to be properly configured.

What am I doing wrong? How can I resize the PCIE windows?

0 Kudos
Reply
1 Solution
2,680 Views
Yuri
NXP Employee
NXP Employee

@lmendes 
Hello,

  I've sent some comments directly.

Regards,
Yuri.

View solution in original post

4 Replies
2,726 Views
Yuri
NXP Employee
NXP Employee

@lmendes 
Hello,

   You mentioned about PCIEA  larger with 256MB MEM window - according to
Table 2-2 (System memory map) of the preliminary i.MX8QM RM, only 256MB are
reserved in system memory for PCIe0 and 256MB - for PCIe1.

Regards,
Yuri.

0 Kudos
Reply
2,710 Views
lmendes
Contributor III

Hi Yuri,

Thanks for your reply.

 

Is it possible to change the Linux memory mappings to extend the PCIe size? I would need one PCIe with 256MB memory BAR excluding the IO BAR size, but I only need 256MB memory BAR on one PCIe and the other PCIe can be shrinked, so that in total the overall 512MB of the PCIe interfaces isn't exceeded. Unfortunately I don't have access yet to the i.MX8QM RM, or at least was unable to find it.

Regards,

Luís

0 Kudos
Reply
2,681 Views
Yuri
NXP Employee
NXP Employee

@lmendes 
Hello,

  I've sent some comments directly.

Regards,
Yuri.

2,235 Views
jgateizo
Contributor I

Hi Yuri,

I've the same problem, could you share your comments?

Thanks,

Joerg