How to reset IPU3 CSI0 interface on IMX.6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to reset IPU3 CSI0 interface on IMX.6

2,198 次查看
zohanlin
Contributor IV

Dear all,

I use Android 4.2.2 on iMX.6

I want to reset IPU3 CSI0 interface manually when CPU get an interrupt, 

and I run theses functions as below, but they don't work. 

----------------------------------------------------------------------------------------------------------

ipu_disable_csi(&ipu_bk_0, 0);

ipu_disable_channel(&ipu_bk_0, channel_bk_0, 1);

ipu_uninit_channel( &ipu_bk, // The function would initialize some parameters.
channel_bk);

ipu_csi_set_window_size(cam->ipu, cam->crop_current.width,
cam->crop_current.height, cam->csi);


ipu_csi_set_window_pos(cam->ipu, cam->crop_current.left,
cam->crop_current.top,
cam->csi);


ipu_csi_init_interface(cam->ipu, cam->crop_bounds.width,
cam->crop_bounds.height,
pixelformat_bk1, csi_param_bk1);

ipu_init_channel( &ipu_bk_0,
channel_bk_0,
params_bk_0_test);

ipu_init_channel_buffer( &ipu_bk_0,
channel_bk_0,
type_bk,
pixel_fmt_bk,
width_bk,
height_bk,
stride_bk,
rot_mode_bk,
phyaddr_0_bk,
phyaddr_1_bk,
phyaddr_2_bk,
u_bk,
v_bk);


ipu_enable_channel(&ipu_bk_0, channel_bk_0);

ipu_enable_csi(&ipu_bk_0, 0);//csi=0

----------------------------------------------------------------------------------------------------------

At first, there are video on display, but when I reset IPU3 CSI0 interface, 

there are no video on display and I got the message :

" imx-ipuv3 imx-ipuv3.0: Warning: channel already initialized 15 "

Could anyone tell me what happened?

Thanks for your reply,

zohan

标签 (1)
0 项奖励
回复
3 回复数

1,905 次查看
igorpadykov
NXP Employee
NXP Employee

Hi zohan

one can check examples of reinitializing ipu in splashscreen patches

https://community.freescale.com/docs/DOC-98109

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,905 次查看
zohanlin
Contributor IV

Hello igor,

Thanks for your patch.

It seems that the patch would reset all ipu,

but we want to reset CSI only.

Is it possible to reset CSI only? 

Thanks,

zohan

0 项奖励
回复

1,905 次查看
igorpadykov
NXP Employee
NXP Employee

Hi zohan

I am afraid this is not possible

Best regards
igor

0 项奖励
回复