How to reset IPU3 CSI0 interface on IMX.6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to reset IPU3 CSI0 interface on IMX.6

2,223件の閲覧回数
zohanlin
Contributor IV

Dear all,

I use Android 4.2.2 on iMX.6

I want to reset IPU3 CSI0 interface manually when CPU get an interrupt, 

and I run theses functions as below, but they don't work. 

----------------------------------------------------------------------------------------------------------

ipu_disable_csi(&ipu_bk_0, 0);

ipu_disable_channel(&ipu_bk_0, channel_bk_0, 1);

ipu_uninit_channel( &ipu_bk, // The function would initialize some parameters.
channel_bk);

ipu_csi_set_window_size(cam->ipu, cam->crop_current.width,
cam->crop_current.height, cam->csi);


ipu_csi_set_window_pos(cam->ipu, cam->crop_current.left,
cam->crop_current.top,
cam->csi);


ipu_csi_init_interface(cam->ipu, cam->crop_bounds.width,
cam->crop_bounds.height,
pixelformat_bk1, csi_param_bk1);

ipu_init_channel( &ipu_bk_0,
channel_bk_0,
params_bk_0_test);

ipu_init_channel_buffer( &ipu_bk_0,
channel_bk_0,
type_bk,
pixel_fmt_bk,
width_bk,
height_bk,
stride_bk,
rot_mode_bk,
phyaddr_0_bk,
phyaddr_1_bk,
phyaddr_2_bk,
u_bk,
v_bk);


ipu_enable_channel(&ipu_bk_0, channel_bk_0);

ipu_enable_csi(&ipu_bk_0, 0);//csi=0

----------------------------------------------------------------------------------------------------------

At first, there are video on display, but when I reset IPU3 CSI0 interface, 

there are no video on display and I got the message :

" imx-ipuv3 imx-ipuv3.0: Warning: channel already initialized 15 "

Could anyone tell me what happened?

Thanks for your reply,

zohan

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,930件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi zohan

one can check examples of reinitializing ipu in splashscreen patches

https://community.freescale.com/docs/DOC-98109

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,930件の閲覧回数
zohanlin
Contributor IV

Hello igor,

Thanks for your patch.

It seems that the patch would reset all ipu,

but we want to reset CSI only.

Is it possible to reset CSI only? 

Thanks,

zohan

0 件の賞賛
返信

1,930件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi zohan

I am afraid this is not possible

Best regards
igor

0 件の賞賛
返信