Hello,
I've found some strange sections in the IMX6SDLRM revision 3.
Namely, in chapters: 9.2.2.2, 9.2.2.3, 9.2.2.4,
there are rate/data throughput specifications listed as:
"up to pixels/sec".
However, in other sections, numbers are given, such as "The data rate is up to 198M pixels/sec" in chapter 9.2.2.1.
To me this looks like someone forgot to put the actual numbers into the reference manual.
Unfortunately, I couldn't find any description of how to report the issues with the documentation within the reference manual itself, so I'm asking here.
已解决! 转到解答。
Hello,
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer
button. Thank you!
Hello,
more details from the team:
Multimedia chapter > Section Video de-interlacer (VDIC)
Bullet: • Rate: up to pixels/sec. should read • Rate: up to 198M pixels/sec.
Multimedia chapter > Section Image Converter (IC) > Data throughput bullets should read:
• For a single active task: up to 240M pixels/sec for input and up to 120M pixels/sec for output.
• For several active tasks: up to 200M pixels/sec for input and up to 100M pixels/sec for output.
Multimedia chapter > Section Image Rotator (IRT) > Data throughput bullets should read:
• When a single task is active: up to 120M pixels/sec.
• When more tasks are active: up to 100M pixels/sec.
Created ticket for documentation correction.
Regards,
Yuri.
Hello,
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer
button. Thank you!