I'm using an imx6slevk board with yocto bsp and I've observed that I need to hold down the power button (on our custom keypad) for 5 seconds to power off the device, Is there anyway I can reduce this time to 1 second? will reducing this effect other functionalities like waking the lcd console when it enters into blank state after 15 minutes of inactivity?
I've found a logind.conf file in systemd (/etc/systemd/logind.conf)
where these two lines caught my eye
#InhibitDelayMaxSec=5
#HandlePowerKey=poweroff
I changed the delay to 1 but there is no change in the power off time
Is there any driver file I need to modify to achieve this?