How to record audio with iMX6 Sabre SDP built-in microphones

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to record audio with iMX6 Sabre SDP built-in microphones

3,100 次查看
bonzo
NXP Employee
NXP Employee

Hello,

The Sabre SDP has two digital microphones.  They are Analog Devices ADMP421B which are connected to a Wolfson WM8962 Codec.

What Linux command do I use to record audio? 

Alsa or gstreamer?  And how would I switch between built-n microphones to microphone input jack?

Any help would be appreciated.

Thank you.

标签 (1)
标记 (4)
3 回复数

1,561 次查看
Yuri
NXP Employee
NXP Employee

Please use section 23.5.1 (Stereo CODEC Unit Test) of "i.MX_6Dual6Quad_Linux_Reference_Manual.pdf".

https://www.freescale.com/webapp/Download?colCode=L3.0.35_4.1.0_LINUX_DOCS&location=null&fpsp=1&Pare...

1,561 次查看
bonzo
NXP Employee
NXP Employee

Thank you Yuri.

Brad

0 项奖励
回复

1,561 次查看
YixingKong
Senior Contributor IV

Bradley

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help please feel

free to contact Freescale.

Thanks,
Yixing

0 项奖励
回复