How to read iMX28 registers from Linux?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to read iMX28 registers from Linux?

跳至解决方案
2,744 次查看
JuanmaAlvarez
Contributor II

Hello,

I need to read some of iMX28 internal registers to check if they have the correct value once Linux is running.

Any ideas?

/dev/mem starts at address 0x100000000, I need to read 0x8... ....

Regards

1 解答
2,345 次查看
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Juan,

I use the memtool. You can find it under the root@freescale /unit_tests$ folder. Or, if you don't have it installed, you can use the attached memwatch.

Best regards.

Jorge.

在原帖中查看解决方案

2 回复数
2,346 次查看
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Juan,

I use the memtool. You can find it under the root@freescale /unit_tests$ folder. Or, if you don't have it installed, you can use the attached memwatch.

Best regards.

Jorge.

2,345 次查看
JuanmaAlvarez
Contributor II

Thanks!!!

It works!!!

Thank you very much! :smileyhappy:

0 项奖励
回复