How to program the BOOT_CFG1[7:4] eFUSEs to select the boot device

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to program the BOOT_CFG1[7:4] eFUSEs to select the boot device

1,440 次查看
adityanagal
Contributor III

Hi ,

I am working on the IMX6 solo based target board. I need to select the external boot device. So how to program  BOOT_CFG1[7:4] eFUSEs to select the boot device . Do we need JTAG or some other hardware tool to program these fuses. Please provide the details. Thanks!

Regards,

Aditya Nagal

0 项奖励
回复
1 回复

1,022 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Aditya

fuses can be blown in uboot:

https://community.freescale.com/docs/DOC-95458

http://boundarydevices.com/fuse-command/

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复