How to prepare Android root file system?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to prepare Android root file system?

2,411 次查看
jiaoka010
Contributor I

I'm working a custom board based on i.MX6Q. Now, I already have a working Androdified kerne. How do I prepare the Jelly Bean root file system? And how do I partition and copy over the RFS to the SD card?

标签 (3)
0 项奖励
回复
3 回复数

2,158 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Jiao,

     We provide MFG Tools to cusotmer for burning android images and linux images into SD card and Flash on board. Did you try to use it ?  As for android RF, you can refer to mx6 sabreSD board and create a new RF for cusotmer board. when you run "source build.....", the customized board can be included, then lunch it.

Regards,

Weidong

0 项奖励
回复

2,158 次查看
jiaoka010
Contributor I

Last time I checked, the MFG Tools requires me to connect the board, so I assume it only works for Freescale reference board, am I wrong? What are the steps to use it to burn Android image to any SD card?

Can I lunch for sabreSD and then use the generated RF plus my own Android kernel? In case some modifications are needed, which file I need to look at? Hope you can provide some directions for me as I'm very to Android porting.

0 项奖励
回复

2,158 次查看
LeonardoSandova
Specialist I

For this particular question: "What are the steps to use it to burn Android image to any SD card?" You can use the script ' fsl-sdcard-partition.sh' located on the source tarball. This way, you do not need the MFGtool, just a Linux host with the SD card.

0 项奖励
回复