How to port RTLinux on iMX6 board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to port RTLinux on iMX6 board

6,207 次查看
shalinikp
Contributor II

Can anyone please let me know if we can port RTLinux on IMX.6 as we need an RTOS for developing realtime applications on IMX.6 board. Also need support on how to get the source and port it

标签 (3)
9 回复数

3,958 次查看
abdelrahmanzaye
Contributor III

Hi ,

i need to choose the best compatible rtos for IMX6-quad
can you kindly  help me ?

0 项奖励
回复

3,959 次查看
igorpadykov
NXP Employee
NXP Employee

Hi shalini

below some links for RT linux

https://rt.wiki.kernel.org/index.php/Main_Page

http://bis-linux.com/files/EUF-ENT-T0866_BIS-Embedded_Linux_for_i.MX-Real-World_Projects.pdf

and new i.MX6 processor which will support MQX

http://linuxgizmos.com/freescale-to-add-cortex-m4-to-imx6-for-automotive-soc/

Regarding support for porting suggest link below

Professional Engineering Services|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

3,959 次查看
jppoulin
Contributor III

Hi!  Has there been any development on RTLinux on the MX6?

Has anyone been able to construct a robust RTLinux system on this platform?  (I do not see any Freescale chips listed in the 'tested RTLinux' platforms at https://rt.wiki.kernel.org/index.php/CONFIG_PREEMPT_RT_Patch#Platforms_Tested_and_in_Use_with_CONFIG...)

Jean-Pierre

0 项奖励
回复

3,959 次查看
sinanakman
Senior Contributor III

Hi Jean-Pierre

For whatever it is worth, I took a recent RT patch set sometimes

ago and ran it on a sabre sd board. I was doing some audio related

tests and it seemed pretty stable to me.

Hope this helps.

Regards

Sinan Akman

3,959 次查看
jppoulin
Contributor III

Hi Sinan, thanks for that input.

If audio is working well under a loaded RTLinux system that is an excellent test!

I wonder if RTLinux is as functional on the MX28 & MX25 we're using...

Thanks!  :smileyhappy:

0 项奖励
回复

3,959 次查看
sinanakman
Senior Contributor III

Hi Jean-Pierre

I just dug up a bit to see what I did earlier.

It seems I took 3.14.3-rt5 for testing some

latencies with RT.

I have also an imx28eval board that I

can give this a try. This week is a bit too

busy but perhaps next week. Let me know

if you haven't done this by yourself by that

time.

Regards

Sinan Akman

3,959 次查看
jppoulin
Contributor III

Hi Sinan, thank you very much for that offer.  That would be valuable information.

It's good to know that there is kernel-level support and that it 'should work'.  I am not well versed into how to properly test if RTLinux works on embedded board, so if you happen to be working on the MX28 and its not too much hassle that would be very useful!

Thanks! 

0 项奖励
回复

3,959 次查看
jppoulin
Contributor III

Oh thanks Igor for taking the time with these great links! :-)

0 项奖励
回复