How to mount yaffs on NAND

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to mount yaffs on NAND

1,972件の閲覧回数
jvidalsm
Contributor I

Hi everyone,

I have a iMX6 Q processor whit NAND flash.

The NAND uses ubifs like file system.

According the source code, I have two methods to mount a system.img

Used for NAND: device/fsl/imx6/etc/fstab_nand.freescale

----------------------------------------------------------------------------------

ubi0:system    /system    ubifsrowait

ubi0:data       /data           ubifs   nosuid,nodev,nodiratime,noatime         wait

ubi0:cache      /cache          ubifs   nosuid,nodev                            wait

ubi0:device     /device         ubifs   nosuid,nodev                         wait

Used for SD-card: device/fsl/imx6/etc/fstab.freescale

-------------------------------------------------------------------------------

/dev/block/mmcblk0p5    /system  ext4    ro                                                                               wait

/dev/block/mmcblk0p4    /data    ext4    nosuid,nodev,nodiratime,noatime,nomblk_io_submit,noauto_da_alloc,errors=panic    wait,encryptable=footer

/dev/block/mmcblk0p6    /cache   ext4    nosuid,nodev,nomblk_io_submit                          wait

/dev/block/mmcblk0p7    /device  ext4    ro,nosuid,nodev

I have a system.img file which uses yaffs like file system.

How I make to mount the system.img file to mount point. I mean, to  "/system" ?

I hope for your help.

Thanks in advance.

Best regards.

jvidalsm

ラベル(2)
タグ(5)
0 件の賞賛
返信
0 返答(返信)