Dear,
The board using i.mx6ull, and linux starts from Nandflash.
I used MFGTool to burn Uboot, kernel and rootFS, which can be started normally.
Now I want to modify uboot or kernel burning addresses, but I did not find out how to operate in "IMX6ULLRM" and "i.mx_linux_user 's_Guide", could you help me solve this case?
Looking forward to your reply.
Hi Jack
NAND uses FCB structure which contains the page address for
primary and secondary boot images. Table 8-11. Flash control block structure
i.MX6ULL Reference Manual describes Firmware1_startingPage: Page number
address where the first copy of bootable firmware is located.
in uboot/include/configs/mx6ul_14x14_evk.h one can check
#define CONFIG_MFG_NAND_PARTITION
Mfg Tool uses ucl2.xml script and kobs-ng for writing uboot to nand partitions.
cafatgithub/imx-kobs - i.MX tool for flashing NAND boot to nand flash
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
could you clarify what "address" do you mean ?
Best regards
igor
you can look at first answer describing procedure of flashing nand image,
in particular ucl2.xml script. Unfortunately I can not understand what "address" do you mean.
Best regards
igor
For example, MFG burns uboot to 0x100000 of Nand Flash, the system can start normally, but I want to change the address to 0x5000000, what do I need to change? ucl2.xml script? Boot PIN? Uboot source code?
In addition, if the uboot of i.mx6ull must burn to 0x100000 of Nand Flash, which document has instructions about the Flash Map(Uboot address, kernel address, DTB address, rootfs address etc..)
Thanks.
could you show in documenation or sources where MFG burns uboot to 0x100000.
In general there is no good nand programming documentation, most detailed is Reference Manual.
If "address" question refers to uboot addresses one can look at some uboot explanations:
arm - Understanding Linux load address for U-Boot process - Stack Overflow
Best regards
igor
Thanks Igorpadykov ,
Our concerns are as follows:
Actually, booting from nand flash , we found out the uboot should be located at 0x100000 in the nand flash.
The address should be modify to any other address, we hope that the uboot can be located in the first nand flash block.