How to modify u-boot device tree for a custom board based on iMX91 with yocto

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to modify u-boot device tree for a custom board based on iMX91 with yocto

跳至解决方案
2,395 次查看
RD-airzone
Contributor II

Hello NXP team,

I'm trying to build a custom image for my custom board. It is based on iMX91 so I've created a new machine copying configuration from evaluation board. I've also add a copy of the EV board device tree (named ws-hub.dts) to the u-boot-imx recipe and change the model name to something else, just to know it is using it. In addition, I've created succesfully a bbappend to add the custom DT to Makefile under "CONFIG_ARCH_IMX9" option.

Then I've created a "airzone_uboot_defconfig" file for my machine based on imx91_11x11_evk_defconfig and modify on my machine conf the variable "UBOOT_CONFIG_BASENAME" to "airzone_uboot". I can see that it is being compiled succesfully

If I leave it as it is, if flashs correctly and then loads kernel but it is not using my custom DT.

Then, I've modify "CONFIG_DEFAULT_FDT_FILE" from defconfig to ws-hub.dtb and it tells "Failed to load 'ws-hub.dtb' ".

I've checked the command "fdt list" on uboot to see the device tree but it show me this:

u-boot => fdt list
/ {
interrupt-parent = <0x00000001>;
#address-cells = <0x00000002>;
#size-cells = <0x00000002>;
model = "NXP i.MX91 11X11 EVK board";
compatible = "fsl,imx91-11x11-evk", "fsl,imx91";
aliases {
};
cpus {
};
clock-osc-32k {
};
clock-osc-24m {
};
clock-ext1 {
};
pmu {
};
thermal-zones {
};
psci {
};
timer {
};
interrupt-controller@48000000 {
};
usbphynop1 {
};
usbphynop2 {
};
soc@0 {
};
imx93-lpm {
};
se-fw2 {
};
chosen {
};
reserved-memory {
};
regulator-can2-stby {
};
regulator-adc-vref {
};
regulator-usdhc2 {
};
regulator-vdd-12v {
};
regulator-vrpi-3v3 {
};
binman {
};
firmware {
};
backlight {
};
panel {
};
signature {
};
__symbols__ {
};
};

So I don't know where that device tree comes from.

My question is how am I suppose to modify the u-boot to adapt it to my board? Am I on the right way or do I have to modify directly the evaluation board DT?

I post my machine.conf in case that you need for reference:

MACHINEOVERRIDES =. "mx91:"

require conf/machine/include/imx-base.inc
require conf/machine/include/arm/armv8-2a/tune-cortexa55.inc
 
DDR_FIRMWARE_NAME = " \
    lpddr4_dmem_1d_v202201.bin \
    lpddr4_dmem_2d_v202201.bin \
    lpddr4_imem_1d_v202201.bin \
    lpddr4_imem_2d_v202201.bin \
"

# Remove unused image types
IMAGE_FSTYPES:remove = "wic.bmap"
IMAGE_FSTYPES:remove = "tar.zst"

MACHINE_FEATURES += "pci wifi bluetooth"
MACHINE_FEATURES:append:use-nxp-bsp = " dpdk optee nxpwifi-all-sdio"
 
# No cares about kernel device tree right now
# KERNEL_DEVICETREE_BASENAME = "imx91-11x11-evk"
# KERNEL_DEVICETREE = "freescale/${KERNEL_DEVICETREE_BASENAME}.dtb"

# Select NXP U-Boot.
IMX_DEFAULT_BOOTLOADER:use-nxp-bsp = "u-boot-imx"

LOADADDR = ""
UBOOT_SUFFIX = "bin"
UBOOT_MAKE_TARGET = ""

SPL_BINARY = "spl/u-boot-spl.bin"

UBOOT_CONFIG ??= "sd"
#UBOOT_CONFIG_BASENAME = "imx91_11x11_evk"
UBOOT_CONFIG_BASENAME = "airzone_uboot"
UBOOT_CONFIG[sd]   = "${UBOOT_CONFIG_BASENAME}_defconfig,sdcard"

# Set ATF platform name
ATF_PLATFORM = "imx91"

IMXBOOT_TARGETS = "flash_singleboot"

IMX_BOOT_SOC_TARGET = "iMX91"
IMX_BOOT_SEEK = "32"

# We have to disable SERIAL_CONSOLE due to auto-serial-console
SERIAL_CONSOLES = "115200;ttyLP0"

IMX_DEFAULT_BSP = "nxp"
Thank you for your time.

 

标签 (1)
标记 (4)
1 解答
2,235 次查看
RD-airzone
Contributor II

Hi everyone,

I post what it actually happens just in case anyone has the same issue.

I had to change CONFIG_DEFAULT_DEVICE_TREE as @Manuel_Salas said but I had to include "imx91-11x11-evk-u-boot.dtsi" at the end of my device tree as it seems to do some configuration needed for u-boot.

 

Kind regards.

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,236 次查看
RD-airzone
Contributor II

Hi everyone,

I post what it actually happens just in case anyone has the same issue.

I had to change CONFIG_DEFAULT_DEVICE_TREE as @Manuel_Salas said but I had to include "imx91-11x11-evk-u-boot.dtsi" at the end of my device tree as it seems to do some configuration needed for u-boot.

 

Kind regards.

0 项奖励
回复
2,358 次查看
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @RD-airzone 

I hope you are doing very well.

 

Could you please try changing the CONFIG_DEFAULT_DEVICE_TREE?

 

Best regards,

Salas.

0 项奖励
回复
2,329 次查看
RD-airzone
Contributor II

Hi @Manuel_Salas,

If I change that setting, I cannot even flash the uboot with:

./uuu -b emmc .\imx-boot-ws-hub-sd.bin-flash_singleboot

The same command works with the default value (imx91-11x11-evk-tianma-wvga-panel) for CONFIG_DEFAULT_DEVICE_TREE.

 

Best regards.

0 项奖励
回复
550 次查看
galba
Contributor I

Hi @RD-airzone 

I'm an Airzone Webserver (Aircloud Wi-Fi) user.

On October 18th, this motherboard attempted to update from your version 4.15 to 4.20 and experienced an error during the process

The webserver you run on this motherboard stopped reporting information to Airzone Cloud, and I can't use the app. The webserver continues to connect to my Wi-Fi network without issue, although it has little activity.

I have SSH connectivity, but I don't have a username and password to send you logs.

Your technical support has kindly denied me the right to repair and only offered to sell me another motherboard. Is there a way I can correct this failed update?

0 项奖励
回复
478 次查看
RD-airzone
Contributor II

Hello @galba,

We can see your case but this isn't the right place to discuss it. May you provide me a contact email?

Kind regards.

 

 

0 项奖励
回复