Hi,
Can I modify the u-boot configuration after booting into the Linux? I don't want to do that by entering into the u-boot setting prompt to do this.
Thanks...
Hank
已解决! 转到解答。
Hi Huazhi,
Even I also referred the same link which u provided in above query. For getting the "fw_setenv", do the following steps.
In uboot:
1) give 'env' (optional parameter) in uboot and compile it
2) this will generate the 'fw_printenv' in the U-Boot directory tools/env
3) Copy the fw_env.config file too.
3) follow the next steps from the "U-boot environment variables in linux link"
Please let me know any additional details you want for fw_printenv and fw_setenv.
Best regards
Ajith P V
Hi Huazhi
While I am building the u-boot with env option i am getting some error. May be some tool chain issue. i am compiling with cross-compiler tools from Android.
ln -s ../../lib_generic/crc32.c crc32.c
crc32.c:14:20: error: stdint.h: No such file or directory
fw_env.c:27:19: error: errno.h: No such file or directory
fw_env.c:28:19: error: fcntl.h: No such file or directory
fw_env.c:29:19: error: stdio.h: No such file or directory
fw_env.c:30:20: error: stdlib.h: No such file or directory
fw_env.c:32:20: error: string.h: No such file or directory
fw_env.c:33:23: error: sys/types.h: No such file or directory
fw_env.c:34:23: error: sys/ioctl.h: No such file or directory
fw_env.c:35:22: error: sys/stat.h: No such file or directory
fw_env.c:36:20: error: unistd.h: No such file or directory
fw_env.c:43:27: error: mtd/mtd-user.h: No such file or directory
fw_env_main.c:42:19: error: stdio.h: No such file or directory
fw_env_main.c:43:20: error: string.h: No such file or directory
fw_env_main.c:44:20: error: stdlib.h: No such file or directory
/home/vijay/build/ch10-2.2/prebuilt/linux-x86/toolchain/arm-eabi-4.4.0/bin/arm-eabi-gcc -Wall -DUSE_HOSTCC -I/home/vijay/work/allgo/env_uboot/uboot-imx/include crc32.c fw_env.c fw_env_main.c -o fw_printenv
crc32.c:14:20: error: stdint.h: No such file or directory
crc32.c:81: error: expected '=', ',', ';', 'asm' or '__attribute__' before 'crc_table'
crc32.c:157: error: expected '=', ',', ';', 'asm' or '__attribute__' before 'crc32'
crc32.c:204: error: expected '=', ',', ';', 'asm' or '__attribute__' before 'crc32_wd'
fw_env.c:27:19: error: errno.h: No such file or directory
fw_env.c:28:19: error: fcntl.h: No such file or directory
fw_env.c:29:19: error: stdio.h: No such file or directory
fw_env.c:30:20: error: stdlib.h: No such file or directory
fw_env.c:32:20: error: string.h: No such file or directory
fw_env.c:33:23: error: sys/types.h: No such file or directory
fw_env.c:34:23: error: sys/ioctl.h: No such file or directory
fw_env.c:35:22: error: sys/stat.h: No such file or directory
fw_env.c:36:20: error: unistd.h: No such file or directory
fw_env.c:43:27: error: mtd/mtd-user.h: No such file or directory
fw_env.c:59: error: expected specifier-qualifier-list before 'ulong'
fw_env.c:69: error: unknown field 'mtd_type' specified in initializer
fw_env.c:69: error: 'MTD_ABSENT' undeclared here (not in a function)
fw_env.c:71: error: unknown field 'mtd_type' specified in initializer
fw_env.c:88: error: expected specifier-qualifier-list before 'uint32_t'
fw_env.c:93: error: expected specifier-qualifier-list before 'uint32_t'
fw_env.c:106: error: expected specifier-qualifier-list before 'uint32_t'
fw_env.c:113: error: unknown field 'flag_scheme' specified in initializer
fw_env.c:219: error: expected '=', ',', ';', 'asm' or '__attribute__' before 'getenvsize'
fw_env.c: In function 'fw_getenv':
fw_env.c:239: error: 'struct environment' has no member named 'data'
fw_env.c:243: error: 'struct environment' has no member named 'data'
Thanks
Vijay
Hi Huazhi,
Please do the changes which navanisrivastava mentioned in the reply. You have to change the fw_env.config with respect to your system modification rather than simply putting it into /etc. you can easily check this from /proc/mtd.
Once you configure the appropriate values in fw_env.config, then rest of the stuffs are pretty easy and same....
Best regards
Ajith P V
Hi Ajith,
Thanks for you reply again. Actually I have done some research about the config file. Here is the link I referred to...
bootloaders:u-boot:env [Analog Devices | Mixed-signal and Digital Signal Processing ICs]
My configuration is
# MTD device name Device offset Env.size Flash sector size number of sectors
/dev/mtd0 0xC0000 0x2000 0x2000
And fw_printenv always reported CRC error here.
Here is my console
root@freescale /media$ cat /proc/mtd
dev: size erasesize name
mtd0: 01000000 00080000 "bootloader"
mtd1: 00500000 00080000 "nand.kernel"
mtd2: 10000000 00080000 "nand.rootfs"
mtd3: 10000000 00080000 "nand.userfs1"
mtd4: 1eb00000 00080000 "nand.userfs2"
#define CONFIG_ENV_SECT_SIZE (8 * 1024)
#define CONFIG_ENV_SIZE CONFIG_ENV_SECT_SIZE
#if defined(CONFIG_FSL_ENV_IN_NAND)
#define CONFIG_ENV_IS_IN_NAND 1
#define CONFIG_ENV_OFFSET 0x200000
#elif defined(CONFIG_FSL_ENV_IN_MMC)
#define CONFIG_ENV_IS_IN_MMC 1
#define CONFIG_ENV_OFFSET (768 * 1024)
#elif defined(CONFIG_FSL_ENV_IN_SATA)
#define CONFIG_ENV_IS_IN_SATA 1
#define CONFIG_SATA_ENV_DEV 0
#define CONFIG_ENV_OFFSET (768 * 1024)
#elif defined(CONFIG_FSL_ENV_IN_SF)
#define CONFIG_ENV_IS_IN_SPI_FLASH 1
#define CONFIG_ENV_SPI_CS 1
#define CONFIG_ENV_OFFSET (768 * 1024)
#else
#define CONFIG_ENV_IS_NOWHERE
Hi Huazhi,
For fw_env.config, your configuration should contain-
MTD device name- /dev/mtdX
X should be the mtd block number in which your environment address is residing.
Device offset- This would always be 0x0000
Env.size- 0x2000 ( according to CONFIG_ENV_SIZE )
Flash sector size- (CONFIG_ENV_SIZE / Number of sectors)
Number of sectors- (CONFIG_ENV_SIZE / NAND Block Size(get it from datasheet) )
For your reference this is my configuration
| # MTD device name | Device offset Env. size | Flash sector size | Number of sectors |
/dev/mtd1 0x0000 0x100000 0x20000 8
when-
#define CONFIG_ENV_SECT_SIZE | (1024 * 1024) |
and Block Size for my NAND is 128K
Hope it helps.. All the Best :smileyhappy::smileyhappy:
Hi Huazhi,
Even I also referred the same link which u provided in above query. For getting the "fw_setenv", do the following steps.
In uboot:
1) give 'env' (optional parameter) in uboot and compile it
2) this will generate the 'fw_printenv' in the U-Boot directory tools/env
3) Copy the fw_env.config file too.
3) follow the next steps from the "U-boot environment variables in linux link"
Please let me know any additional details you want for fw_printenv and fw_setenv.
Best regards
Ajith P V
Hi Huazhi,
Please check fw_env.config file ( u-boot/tools/env/fw_env.config) and make required changes related to env size, Flash sector size and Number of sectors according to flash which you are using. I got similar error but on changing mentioned parameters i got desired output.
Hi,
How can I get the env size, Flash sector size and Number of sectors according to flash which I am using. I have a ls1021a-twr eva board and it's boot from SD card. I do not know how to set the right value in the fw_env.config
Please refer to my post here
I have tried to dump the "Uboot area" on the sd card. But the address of the uboot parameter turns to be different for different configurations.
I saw that there is a uboot utils which can do this easily and I enabled this option in my BSP build. But it just doesn't have that tool. Here is the link of the tool I'm talking about.