How to map DDR on PCI address space?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to map DDR on PCI address space?

1,773 Views
vm18553
Contributor II

Hi,

I'm new to PCI, I've following scenario where I need to map DDR memory into PCI address space,

In Custom board,

FPGA is connected via PCIe.
DMAC will be loaded on the PCIe to offload memory transfer between DDR to PCIe.

Question is how mapping of DDR on PCI address space happening ?

Could you please refer if any API available to do that?

pcie_mapping.png

Thanks,

Vishnu

Labels (2)
0 Kudos
Reply
2 Replies

1,549 Views
vm18553
Contributor II

Dear Igor,

Thanks for sharing link. This link has information about RC validation and doesn't have any information about mapping DDR memory into PCI address space.

Thanks,

Vishnu

0 Kudos
Reply

1,549 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vishnu

please check examples on

https://community.freescale.com/docs/DOC-95014 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply