MCIMX6Q-SDP battery application issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX6Q-SDP battery application issues

1,369 Views
felixhsu
Contributor III

Hi All

Hardware: MCIMX6Q-SDP

Software: Android_JB4.3_1.1.0

Use battery power supply application issues as below,

1. Could modification battery detect voltage? if yes, How to change it.

2. What is the minimum current requirement, when the power from DC in switch to battery?

Thanks.

Labels (6)
Tags (1)
0 Kudos
Reply
1 Reply

1,224 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Felix,

>>1. Could modification battery detect voltage? if yes, How to change it.

On SabreSDP board, 2 MAX8903C chargers was used, the chager IC can only charge battery with 4.2V full voltage, so voltage that needs to be detected should be max 4.2V, if you are using Li battery with 3.6V, you don't need to do any modification.

>>2. What is the minimum current requirement, when the power from DC in switch to battery?

At differenct charging stage, Charging current is different, it is determined by charger IC, so you had better read MAX8903C datasheet carefully.


Have a great day,
TIC  Weidong

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply