How to map DDR on PCI address space?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to map DDR on PCI address space?

2,376件の閲覧回数
vm18553
Contributor II

Hi,

I'm new to PCI, I've following scenario where I need to map DDR memory into PCI address space,

In Custom board,

FPGA is connected via PCIe.
DMAC will be loaded on the PCIe to offload memory transfer between DDR to PCIe.

Question is how mapping of DDR on PCI address space happening ?

Could you please refer if any API available to do that?

pcie_mapping.png

Thanks,

Vishnu

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

2,152件の閲覧回数
vm18553
Contributor II

Dear Igor,

Thanks for sharing link. This link has information about RC validation and doesn't have any information about mapping DDR memory into PCI address space.

Thanks,

Vishnu

0 件の賞賛
返信

2,152件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vishnu

please check examples on

https://community.freescale.com/docs/DOC-95014 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信