How to make sabresd_6dp_eink-eng

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to make sabresd_6dp_eink-eng

2,774 Views
hiroyukihara
Contributor III

I created an environment of android 7.1 using "MCIMX6DL-SDP + IMXEBOOKDC4-EPD".


However, even if I enter the lunch command, "sabresd_6dp_eink-eng (user)" does not appear.

(Created by referring to AndroidTM User's Guide Document Number: AUG Rev. N 7.1.1 - 1.0.0, 03/2017)

The source used is below.
  android_N7.1.1_1.0.0_source.tar.gz

How can I get sabresd_6dp_eink-eng (user) on lunch?

hara@hara-XPS-8300:~/myandroid-7.1$ lunch

You're building on Linux

Lunch menu... pick a combo:
1. aosp_arm-eng
2. aosp_arm64-eng
3. aosp_mips-eng
4. aosp_mips64-eng
5. aosp_x86-eng
6. aosp_x86_64-eng
7. full_fugu-userdebug
8. aosp_fugu-userdebug
9. sabresd_6dq-eng
10. sabresd_6dq-user
11. sabreauto_6q-eng
12. sabreauto_6q-user
13. evk_6sl-eng
14. evk_6sl-user
15. sabresd_6sx-eng
16. sabresd_6sx-user
17. sabreauto_6sx-eng
18. sabreauto_6sx-user
19. evk_6ul-eng
20. evk_6ul-user
21. sabresd_7d-eng
22. sabresd_7d-user
23. sabreauto_8dq-eng
24. sabreauto_8dq-user
25. mini_emulator_arm64-userdebug
26. m_e_arm-userdebug
27. m_e_mips-userdebug
28. m_e_mips64-eng
29. mini_emulator_x86-userdebug
30. mini_emulator_x86_64-userdebug
31. aosp_dragon-userdebug
32. aosp_dragon-eng
33. aosp_marlin-userdebug
34. aosp_sailfish-userdebug
35. aosp_flounder-userdebug
36. aosp_angler-userdebug
37. aosp_bullhead-userdebug
38. hikey-userdebug
39. aosp_shamu-userdebug

Labels (2)
0 Kudos
Reply
4 Replies

2,495 Views
hiroyukihara
Contributor III

Hi Diego

Please reply.

0 Kudos
Reply

2,495 Views
diegoadrian
NXP Employee
NXP Employee

Hello,


The only supported build names are the one that is in the document. You only need to use the sabresd_6dq-user build name an change the boot args to boot from an epdink display.


However, your board probably does not support an EPDINK display. Can you please provide me the complete part number?


Moreover, since Android Ice Cream Sandwich that we do not support the ink display for our Android releases. For that, I recommend you to use a Linux distribution (Yocto).


Best Regards,

Diego.

0 Kudos
Reply

2,495 Views
hiroyukihara
Contributor III

Currently, MCIMX6DL-SDP + IMXEBOOKDC4-EPD
I am working with android4.4.2 + Patch.
(EPD has changed to 13.3 inch)

In the demo image of Android 7.1.1
  u boot-imx7d-epdc.imx
  boot-imx7d-epdc.img
  recovery-imx7d-epdc.img
It contains.
i.MX 7 and i.MX 6 are the same source

How do you create an epdc version?

0 Kudos
Reply

2,495 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

I apologize for the late answer.

First of all the demo image that you have is for the i.mx7d not for the i.mx6dl. Unfortunately, we also do not give support for that image, since is an alpha image. Moreover, I get notified that we do not support the epdink display for Android distributions because we do not support colorless displays for Android distributions. For that, like I said you before. I recommend you to use our Yocto distributions.

Best Regards,

Diego.

0 Kudos
Reply