How to make rootfs?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to make rootfs?

3,972件の閲覧回数
mingmingyuan
Contributor III

dear FSL:

my project info as follow:

board:sambaSD

system:linux 3.0.35

I want to add my app into rootfs, but I don't know how to make rootfs?

ラベル(2)
0 件の賞賛
返信
6 返答(返信)

3,409件の閲覧回数
saurabh206
Senior Contributor III

Hi Yuan,

With LTIB also you should have rootfs generated.

Also you can use debian or ubuntu rootfs.

0 件の賞賛
返信

3,409件の閲覧回数
mingmingyuan
Contributor III

Thank you for your help!

document that you give me description how to add app code to ltib, but doesn't introduce how to make rootfs.

I found flash tool Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER include rootfs file name is  rootfs.tar.bz2. this rootfs file works fine.

Can you guide me that how to create rootfs.tar.bz2 file?

0 件の賞賛
返信

3,409件の閲覧回数
bpe
NXP Employee
NXP Employee

Just invoke ltib without arguments. If you have changed the configuration or made a cleanup, ltib will rebuild the target.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,409件の閲覧回数
saurabh206
Senior Contributor III

Hi Yuan

You can use the Yocto Project to prepare custom rootfs.

Check following link.

Yocto Training - HOME

Thanks

Saurabh

0 件の賞賛
返信

3,409件の閲覧回数
mingmingyuan
Contributor III

dear sir:

I use ltlib, not yocto!

0 件の賞賛
返信

3,409件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi mingming

for ltib pllease look at document

pdk2009_12_imx25_Linux_HelloWorld_AN.pdf

included in

IMX25_0912_SDK_LINUXDOCS_BUNDLE

i.MX25 SDK 2009.12 Linux Documentation Bundle

Best regards

igor

0 件の賞賛
返信