How to load Neutron Delegate library on i.MX 95.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to load Neutron Delegate library on i.MX 95.

553 次查看
DennisTseng
Contributor II

Hi team,

I'm using the Linux 6.6.36 on imx95-19x19-lpddr5-evk board.

I tried to run a python script to confirm different platform performance by using simple case of the ResNet50 model and convert to TensorFlow Lite to do inference.

I followed the i.MX Machine Learning User's Guide that mentioned about if I want to run the inference using the GPU/NPU hardware accelerator, need to use the --external_delegate_path switch: 

• For VX Delegate on i.MX 8: --external_delegate_path=/usr/lib/libvx_delegate.so
• For Ethos-U Delegate on i.MX 93: --external_delegate_path=/usr/lib/libethosu_delegate.so
• For Neutron Delegate on i.MX 95: --external_delegate_path=/usr/lib/libneutron_delegate.
so

And I also run this example is working well, but my script have different way between this example code about load the external delegate.

here is the part in my script :

 

 

import tensorflow as tf
class VelaInference(InferenceBase):
    def __init__(self, model_loader, model_path, debug_mode=False):
        """
        Initialize the VelaInference object.

        :param model_loader: Object responsible for loading the model and categories.
        :param model_path: Path to the tflite model.
        :param debug_mode: If True, print additional debug information.
        """
        
        super().__init__(model_loader, vela_path=model_path, debug_mode=debug_mode)

    def load_model(self):
        num_threads=os.cpu_count()
        print("num_threads=",num_threads)
        delegates = []
        
        for _ in range(2):
            try:
                self.interpreter = tf.lite.Interpreter(
                    model_path=self.vela_path,
                    num_threads=num_threads,
                    experimental_delegates=delegates,
                )

                self.interpreter.allocate_tensors()
            except RuntimeError as re:
                if len(
                    delegates
                ) == 0 and "Encountered unresolved custom op: ethos-u." in str(re):
                    # retry with the Ethos-U delegate
                    print("using libethosu_delegate")
                    delegates = [tf.lite.experimental.load_delegate("/usr/lib/libethosu_delegate.so")]
                    continue

                raise re

        input_details = self.interpreter.get_input_details()
        output_details = self.interpreter.get_output_details()

        self.input_index = input_details[0]["index"]
        self.output_0_index = output_details[0]["index"]
        print('input: ', self.input_index)
        print('output: ', self.output_0_index)
        print("VelaInference init done.")
    def predict(self, input_data, is_benchmark=False):
....
....

 

 

This load delegate way is working well on i.MX93, but when I change the library path (

/usr/lib/libneutron_delegate.so) and run it on i.MX95 will get error.
 
here is the error log :

 

num_threads= 6
Traceback (most recent call last):
  File "/home/root/resnet50.py", line 498, in <module>
    tflite_vela_inference = VelaInference(
                            ^^^^^^^^^^^^^^
  File "/home/root/resnet50.py", line 290, in __init__
    super().__init__(model_loader, vela_path=model_path, debug_mode=debug_mode)
  File "/home/root/resnet50.py", line 80, in __init__
    self.model = self.load_model()
                 ^^^^^^^^^^^^^^^^^
  File "/home/root/resnet50.py", line 316, in load_model
    raise re
  File "/home/root/resnet50.py", line 300, in load_model
    self.interpreter = tf.lite.Interpreter(
                       ^^^^^^^^^^^^^^^^^^^^
  File "/usr/lib/python3.12/site-packages/tensorflow/lite/python/interpreter.py", line 513, in __init__
    self._interpreter.ModifyGraphWithDelegate(
RuntimeError: Caught an unknown exception!

 

 

What the different between i.MX 93 and 95's delegate library ?

Why 95's delegate library must need to using the specific way like the example script ?

 

0 回复数