How to interface Microcontroller with i.MX6 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to interface Microcontroller with i.MX6 ?

2,743件の閲覧回数
hrushinale
Contributor III

Hello All,

I want interface the Micro-controller (e.g 8051) with i.MX6 solo and I want to read the data from that Micro-controller Over UART.

Kindly Provide me the suggestions or reference for doing the same.

Best Regards,

Hrushi

タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,676件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Hrushi

please check attached document Chapter 45 Universal Asynchronous Receiver/Transmitter
(UART) Driver and examples in imx-test package
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.4.tar.gz

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,676件の閲覧回数
hrushinale
Contributor III

Hello igorpadykov,

Thanks for your reply.

Do you have specific exapmles for UART test driver.

0 件の賞賛
返信