How to interface MCP79402 to imx6ul ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to interface MCP79402 to imx6ul ?

1,037件の閲覧回数
pnaven03
Contributor I

Hi,

We currently using imx6ul board with yocto build system, RTC module (MCP79402) interface to imx6ul board using i2c bus. How to add in device tree and Driver in yocto build. How to set time, date and alarm. Please any one help on this issue.

Regards,

Nk. 

ラベル(1)
0 件の賞賛
返信
1 返信

956件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nk

some MCP79402 drivers can be found on:

br-armadeus/linux-0505-armadeus-add_mcp7940x_rtc_driver.patch at master · trabucayre/br-armadeus · G... 

Yocto Training - home 

BSP porting guide: from a I.mx6q reference Board to a Custom board (in Yocto project) 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信