How to integrate Driver in U-Boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to integrate Driver in U-Boot

2,414 Views
nikhil29
Contributor III

Hello NXP TechSupport

 

I'm working on Custom Board which is based on i.MX 8M Mini Processor.

1] I need to integrate the Driver in U-Boot and Compile it to build its image.

2] Can you please share the detailed procedure step by step.

 

Thanks

Nikhil

 

Labels (1)
0 Kudos
Reply
2 Replies

2,387 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

The key file is

/drivers/Kconfig

/drivers/Makefile

 

Then you can research the example driver:/drivers/ timer

 

BR

Zhiming

0 Kudos
Reply

2,374 Views
nikhil29
Contributor III

Hello Zhiming, Thanks for your time

 

1] I have written Makefile and Kconfig for integrating driver.

2] After that to bind that driver with the bootloader, I used the command,

bitbake -c menuconfig virtual/bootloader, but showing error

 

ERROR:-
========

1] ERROR: u-boot-variscite-1.0-r0 do_configure: Execution of '/home/nikhil/Variscite-DART-MX8M-MINI/var-fsl-yocto/build_xwayland/tmp/work/imx8mm_var_dart-poky-linux/u-boot-variscite/1.0-r0/temp/run.do_configure.17897' failed with exit code 1:
cp: cannot stat '/home/nikhil/Variscite-DART-MX8M-MINI/var-fsl-yocto/build_xwayland/tmp/work/imx8mm_var_dart-poky-linux/u-boot-variscite/1.0-r0/u-boot-variscite-1.0//.config': No such file or directory
WARNING: exit code 1 from a shell command.

ERROR: Logfile of failure stored in: /home/nikhil/Variscite-DART-MX8M-MINI/var-fsl-yocto/build_xwayland/tmp/work/imx8mm_var_dart-poky-linux/u-boot-variscite/1.0-r0/temp/log.do_configure.17897

 

2] ERROR: Execution of '/home/nikhil/Variscite-DART-MX8M-MINI/var-fsl-yocto/build_xwayland/tmp/work/imx8mm_var_dart-poky-linux/u-boot-variscite/1.0-r0/temp/run.do_configure.17897' failed with exit code 1:
| cp: cannot stat '/home/nikhil/Variscite-DART-MX8M-MINI/var-fsl-yocto/build_xwayland/tmp/work/imx8mm_var_dart-poky-linux/u-boot-variscite/1.0-r0/u-boot-variscite-1.0//.config': No such file or directory

 

3] ERROR: Task (/home/nikhil/Variscite-DART-MX8M-MINI/var-fsl-yocto/sources/meta-variscite-imx/recipes-bsp/u-boot/u-boot-variscite.bb:do_configure) failed with exit code '1

 

Please provide a resulting solution for successful driver integration.

 

Thanks

Nikhil

 

0 Kudos
Reply