How to install whl files with pip3?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to install whl files with pip3?

2,264 次查看
SoniaArevalo
Contributor I

I got some wheel packages and I would like to install them with pip3 install comand in a recipe. I can load the whl files, but it is not installed.

My current recipe is as follows:

DESCRIPTION="WHL file"
SRC_URI = "file://XXXXXXX.whl"

S = "${WORKDIR}"

LICENSE="CLOSED"

do_install() {
       install -d ${D}${libdir}/
       install -m 0644 ${S}/XXXXXXX.whl ${D}${libdir}/

       # pip3 install XXXXXXX.whl
}

I would like to know how to add pip3 install command.

Thanks everyone.

标签 (1)
0 项奖励
回复
2 回复数

2,253 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

The bb file should like this:

 

COMPATIBLE_HOST = "i686.*-mingw.*"                                                                  

SRC_URI = "https://files.pythonhosted.org/packages/d8/9d/7a8cad803ef73f47134ae5c3804e20b54149ce62a7d1337204f3cf2d1fa1/MarkupSafe-1.1.1-cp35-cp35m-win32.whl;downloadfilename=MarkupSafe-1.1.1-cp35-cp35m-win32.zip;subdir=${BP}"

SRC_URI[md5sum] = "a948c70a1241389d7120db90d69079ca"                                                
SRC_URI[sha256sum] = "6dd73240d2af64df90aa7c4e7481e23825ea70af4b4922f8ede5b9e35f78a3b1"             

inherit nativesdk python3-dir                                                                       

LICENSE = "BSD-3-Clause"                                                                            

PV = "1.1.1"                                                                                        
PN = "nativesdk-python3-markupsafe"                                                                 

LIC_FILES_CHKSUM = "file:///${S}/MarkupSafe-1.1.1.dist-info/LICENSE.rst;md5=ffeffa59c90c9c4a033c7574f8f3fb75"

do_unpack[depends] += "unzip-native:do_populate_sysroot"                                            

PROVIDES += "nativesdk-python3-markupsafe"                                                          
DEPENDS += "nativesdk-python3"                                                                      

FILES_${PN} += "\                                                                                   
    ${libdir}/${PYTHON_DIR}/site-packages/* \                                                       
"                                                                                                   

do_install() {                                                                                      
    install -d ${D}${libdir}/${PYTHON_DIR}/site-packages/MarkupSafe-1.1.1.dist-info                 
    install -d ${D}${libdir}/${PYTHON_DIR}/site-packages/markupsafe                                 

    install -m 644 ${S}/markupsafe/* ${D}${libdir}/${PYTHON_DIR}/site-packages/markupsafe/          
    install -m 644 ${S}/MarkupSafe-1.1.1.dist-info/* ${D}${libdir}/${PYTHON_DIR}/site-packages/MarkupSafe-1.1.1.dist-info/
}
0 项奖励
回复

2,218 次查看
SoniaArevalo
Contributor I

Many thanks for your answer, but this didn’t work to me.

The whl file is already downloaded so I wrote  a bb file similar as yours:

 

DESCRIPTION="WHL files"

SRC_URI = "file://torch-1.6.0-cp37-cp37m-linux_aarch64.whl"

inherit nativesdk python3-dir

LICENSE = "CLOSED"

PV = "1.6.0"
#PN = "nativesdk-python3"

do_unpack[depends] += "unzip-native:do_populate_sysroot"

PROVIDES += "nativesdk-python-whl"
DEPENDS += "nativesdk-python3"

FILES_${PN} += "\
${libdir}/${PYTHON_DIR}/site-packages/* \
"

do_install(){
install -d ${D}${libdir}/${PYTHON_DIR}/site-packages/torch-1.6.0.dist-info
install -d ${D}${libdir}/${PYTHON_DIR}/site-packages/torch

install -m 644 ${S}/torch/* ${D}${libdir}/${PYTHON_DIR}/site-packages/torch/
install -m 644 ${S}/torch-1.6.0.dist-info/* ${D}${libdir}/${PYTHON_DIR}/site-packages/torch-1.6.0.dist-info/
}

But I got some problems.

 

First, when I add “inherit nativesdk” I get the following error:

 

ERROR: Nothing PROVIDES 'virtual/x86_64-pokysdk-linux-gcc'. Close matches:

virtual/x86_64-pokysdk-linux-gcc-crosssdk

virtual/x86_64-pokysdk-linux-go-crosssdk

virtual/x86_64-pokysdk-linux-g++-crosssdk

ERROR: Required build target 'python-whl' has no buildable providers.

Missing or unbuildable dependency chain was: ['python-whl', 'virtual/x86_64-pokysdk-linux-gcc']

 

Then, if I delete the inherit line the whl does not unpack correctly, so I do not get the such file directory.

 

Please, how could I fix it?

 

Regards,

 

Sonia.

0 项奖励
回复