How to install linux for i.MX6 Board?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to install linux for i.MX6 Board?

ソリューションへジャンプ
5,347件の閲覧回数
joowonkim
Contributor III

Hi everyone.

I want to install the linux on i.MX6 Board.

What need for install? and How to install linux for i.MX6?

please help

Thank you to read.

ラベル(3)
1 解決策
4,044件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

H JooWon

you can two alternatives, first yocto (also please read attached Freescale_Yocto_Project_User's_Guide.pdf)

Yocto Training - HOME

L3.10.53_1.1.0_iMX6QDLS_Bundle : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,

i.MX 6Solo Linux Binary Demo Files and Linux BSP Documentation

second - ltib, for that first read below appnote

http://cache.freescale.com/files/dsp/doc/app_note/AN3875.pdf

the attached files

L3.0.35_4.1.0_ER_SOURCE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,

i.MX 6Solo and i.MX 6Sololite Linux BSP Source Code Files.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
4,045件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

H JooWon

you can two alternatives, first yocto (also please read attached Freescale_Yocto_Project_User's_Guide.pdf)

Yocto Training - HOME

L3.10.53_1.1.0_iMX6QDLS_Bundle : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,

i.MX 6Solo Linux Binary Demo Files and Linux BSP Documentation

second - ltib, for that first read below appnote

http://cache.freescale.com/files/dsp/doc/app_note/AN3875.pdf

the attached files

L3.0.35_4.1.0_ER_SOURCE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,

i.MX 6Solo and i.MX 6Sololite Linux BSP Source Code Files.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

4,044件の閲覧回数
joowonkim
Contributor III

Hi igorpadykov

Thank you reply.

If install the linux on i.MX Board, could operating without SDcard?

thank you.

JooWon

0 件の賞賛
返信
4,044件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JooWon

SD is needed for rootfs, also one can use NAND or nfs instead SD.

Please read Linux User Guide for available options.

~igor

0 件の賞賛
返信