How to install image to eMMC from Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to install image to eMMC from Linux

Jump to solution
3,814 Views
janiscoders
Contributor III

Hi, the question is simple. How to install u-boot, linux kernel and filesystem to eMMC via microUSB from Linux. I know it is possible from Windows using MFG Tools, but is there really no possibility to do it from Linux?

If I attach the microUSB to Linux and call 'lsusb' command, I can see that device is recognized:

     15a2:004e Freescale Semiconductor, Inc.

Should it be attached as some kind a block device and install images using 'dd'? Or is it some other kind of serial device with specific protocol for which there is no application available in Linux.

We just simply want to start manufacturing our product and installing images via Linux seems like a good solution, because now we need a separate Windows machine and someone sitting there and installing images for 1000 pieces.

Labels (2)
Tags (3)
0 Kudos
Reply
1 Solution
2,341 Views
Yuri
NXP Employee
NXP Employee

> ... eMMC via microUSB ...

Is this correct ?

eMMC means (my opinion) (chip = SD interface + NAND ) mounted on a board.  

As for target system deploying on Linux host, please look at the “ucl.xml”

of MFG (Linux) configuration for i.MX53. It shows sequence of (Linux) commands,

which may be adopted for a Linux host. 

View solution in original post

0 Kudos
Reply
1 Reply
2,342 Views
Yuri
NXP Employee
NXP Employee

> ... eMMC via microUSB ...

Is this correct ?

eMMC means (my opinion) (chip = SD interface + NAND ) mounted on a board.  

As for target system deploying on Linux host, please look at the “ucl.xml”

of MFG (Linux) configuration for i.MX53. It shows sequence of (Linux) commands,

which may be adopted for a Linux host. 

0 Kudos
Reply