How to install apt-get on i.mx8m mini linux image

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to install apt-get on i.mx8m mini linux image

11,184 次查看
jefflfree
Contributor III

I put Linux 4.14.78_1.0.0_ga_images_MX8MMEVK onto the i.mx8m mini and it boots just fine.

I want to enable to enable i.mx8m mini evk to function as a WAP by installing hostapd.

Assuming this is possible, what are the steps to install "apt-get" onto the i.mx8m mini. I have a debug terminal to the linux prompt but I am stuck. How do I add applications?

[Maybe you can provide me a pointer to how to add individual components to the SD card like apt-get?]

Jeff

标签 (1)
标记 (1)
0 项奖励
回复
16 回复数

10,118 次查看
jefflfree
Contributor III

Ok. I am able to build an image. However I cannot install hostapd on the target system.

Here are the steps I did trying to get hostapd to the target system:

Added the following to conf/local.conf:

PACKAGE_CLASSES ?= "package_rpm"

EXTRA_IMAGE_FEATURES = "debug-tweaks package-management"

IMAGE_INSTALL_append += " apt hostapd"

Then I ran bitbake:

$ bitbake fsl-image-qt5-validation-imx

and got this:

...rpm-software-management.dnf.git/ does not exist

If I remove package-management, it will build. But then on the target system I cannot install hostapd.

When I read the documentation, it seemed to indicate that I need to create a web-server on the development system (package feed) to serve the packages to the target system. Can someone just supply an example of what I need to do to get hostapd package installed?

Jeff

0 项奖励
回复

10,118 次查看
jefflfree
Contributor III

update: hostapd is on the target system now. I just cannot install other packages from the host system. I guess I will have to leave off package-management for now.

0 项奖励
回复

10,118 次查看
jefflfree
Contributor III

I am finding that to build a linux image, it is exceeding the disk space I have (more than 50GB). Is there an image already build that include apt-get?

0 项奖励
回复

10,118 次查看
joanxie
NXP TechSupport
NXP TechSupport

 you also can refer to the topic as below:

https://community.nxp.com/thread/325384 

0 项奖励
回复

10,118 次查看
jefflfree
Contributor III

I made progress. I did not realize I needed 120GB to build linux!

Here is my recipe using Ubuntu 18.04.2

$ DISTRO=fsl-imx-wayland MACHINE=imx8mmevk source fsl-setup-release.sh -b build-wayland

$ bitbake fsl-image-qt5-validation-imx

$ bunzip2 -dk -f fsl-image-qt5-validation-imx-imx8mmevk.sdcard.bz2
$ sudo dd if=fsl-image-qt5-validation-imx-imx8mmevk.sdcard of=/dev/sdb bs=1M conv=fsync

There was a note that said fsl-imx-wayland and fsl-imx-fb are not supported on i.MX 8. If this applies to imx8mmevk, then should I be using fsl-imx-xwayland ?

I installed to sdcard and I am getting a reset loop over and over. Any clues how to debug this?

resetting ...

 

U-Boot SPL 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df5e4 (Aug 13 2019 - 22:07:34 +0000)

power_bd71837_init

DDRINFO: start lpddr4 ddr init

DRAM PHY training for 3000MTS

check ddr4_pmu_train_imem code

check ddr4_pmu_train_imem code pass

check ddr4_pmu_train_dmem code

check ddr4_pmu_train_dmem code pass

Training PASS

DRAM PHY training for 400MTS

check ddr4_pmu_train_imem code

check ddr4_pmu_train_imem code pass

check ddr4_pmu_train_dmem code

check ddr4_pmu_train_dmem code pass

Training PASS

DRAM PHY training for 100MTS

check ddr4_pmu_train_imem code

check ddr4_pmu_train_imem code pass

check ddr4_pmu_train_dmem code

check ddr4_pmu_train_dmem code pass

Training PASS

DRAM PHY training for 3000MTS

check ddr4_pmu_train_imem code

check ddr4_pmu_train_imem code pass

check ddr4_pmu_train_dmem code

check ddr4_pmu_train_dmem code pass

Training PASS

DDRINFO:ddrphy calibration done

DDRINFO: ddrmix config done

Normal Boot

Trying to boot from MMC1

"Synchronous Abort" handler, esr 0x02000000

elr: 0000000000920000 lr : 00000000007e3fd8

x0 : 0000000000920000 x1 : 000000000000000c

x2 : 000000000000000c x3 : 0000000000000073

x4 : 0000000000000009 x5 : 0000000000000073

x6 : 00000000401ffd6f x7 : 0000000000000003

x8 : 0000000000000338 x9 : 0000000000000002

x10: 000000000091db9c x11: 00000000401ff980

x12: 0000000000000305 x13: 00000000000002f8

x14: 000000000091dbdc x15: 00000000401ff980

x16: 0000000000000000 x17: 00000000000000ff

x18: 000000000091de40 x19: 00000000007f71b0

x20: 00000000007f7150 x21: 0000000000000000

x22: 00000000007f0e70 x23: 000000000091dde0

x24: 00000000007f0e58 x25: 00000000007f7000

x26: 00000000deadbeef x27: 0000000072000000

x28: 0000000000000000 x29: 000000000091dd70

 

Resetting CPU ...

 

resetting ...

 

U-Boot SPL 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df5e4 (Aug 13 2019 - 22:07:34 +0000)

 

Jeff

 

 

0 项奖励
回复

10,118 次查看
jefflfree
Contributor III

ok. I solved the reset loop issue. I had incorrectly written the image to the sdcard.

0 项奖励
回复

10,118 次查看
im_tlau
Contributor II

Hi Jeff,

I'm trying the same thing building imx8mm image for evk board, could you let me know what's your steps/commands of writing the imsage to the sd card?

Thanks!

0 项奖励
回复

10,118 次查看
jefflfree
Contributor III

Assuming you were able to build the image using Yocto.

Note: I am running Ubunto 18.04.2 on VirtualBox with a Shared Folder to my windows laptop

cd build-wayland/tmp/deplay/images/imx8mmevk

# Since the sdcard image is compressed, we need to uncompress it

bunzip2 -dk -f fsl-image-qt5-validation-imx-imx8mmevk.sdcard

cp fsl-image-qt5-validation-imx-imx8mmevk.sdcard /media/sf_VirtualBox_Shared

From Windows, I used Rufus to then take the image from the shared folder and write to sdcard which was plugged into my laptop.

(I found this much easier than doing what some people do where they follow this (Access SD Card on Linux from Windows using VirtualBox | Tech Blog)

Then I physically took sdcard and put it into the evk and booted.

10,118 次查看
im_tlau
Contributor II

Thanks Jeff!

It's interesting that cp command does the job, I use dd to dump my .sdcard image to MicroSD card, my problem was resolved, I had to use own built  fsl-image-validation-imx-imx8mmddr4evk-rootfs.sdcard for my iMX8MM DDR4 EVK board, without ddr4 it won't work.

Also good to know Rufus tool for Windows.

0 项奖励
回复

10,118 次查看
joanxie
NXP TechSupport
NXP TechSupport

we have tested that built fsl-imx-xwayland on ubuntu 16.04 successfully, maybe you can try this, if you don't use sdcard image, how about the demo sdcard image? the same issue?

0 项奖励
回复

10,118 次查看
joanxie
NXP TechSupport
NXP TechSupport

if you need to install hostapd, you should build the image by yourself, you need to add the hostapd in the local.conf, then build the image you need, for more detailed information, you also can refer to the yocto traning document:

https://community.nxp.com/docs/DOC-94849 

0 项奖励
回复

10,118 次查看
jefflfree
Contributor III

Since my post I found a linux manual at https://www.nxp.com/webapp/Download?colCode=imx-yocto-L4.14.98_2.0.0_ga which seems like it talks about uboot etc... Is this the path I should be heading?

0 项奖励
回复

10,118 次查看
joanxie
NXP TechSupport
NXP TechSupport

I couldn't open your link, if you means 4.14.98 linux documents, yes, you can refer to that, you can refer to the yocto user guide, which tell you how to download and build the 4.14.98 source code and get your own image

0 项奖励
回复

10,118 次查看
jefflfree
Contributor III

I found the proper link: https://www.nxp.com/design/i.mx-developer-resources/i.mx-software-and-development-tool:IMX-SW

This is the only one that had the 2019 version of Yocto. Under Linux->Linux L4.14.98_2.0.0 Documentation

Is this what I am supposed to follow?

0 项奖励
回复

10,118 次查看
joanxie
NXP TechSupport
NXP TechSupport

you can refer to the link as below:

https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/embedded-...

the latest version for imx8MM is 4.14.98

0 项奖励
回复

10,118 次查看
jefflfree
Contributor III

thx. So, I am following i.MX Yocto Project User's Guide to build an image.

Will this by default include apt-get or would this be considered "customization"? If so, are there any examples on how to do this?

0 项奖励
回复