How to install & verify lpcscrypt in Ubuntu?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to install & verify lpcscrypt in Ubuntu?

2,123 Views
GanesanGuru
Contributor IV

Hi fellas,

I've downloaded LPCScrypt v2.1.2 as lpcscrypt-2.1.2_57.x86_64.deb.bin and run with root privileges, yet I'm not sure where it has installed or how to access it further.. During installation, it happened as follows:

 

image.png

Labels (1)
0 Kudos
Reply
3 Replies

2,106 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which product are you using?

0 Kudos
Reply

2,101 Views
GanesanGuru
Contributor IV

Hi  @Rita_Wang   ,

I'm using iMX RT1064-EVK board and in order to re-program the onboard debugger LPC4322 using  AN13206 , I'm in need of the lpcsrypt . I'm installing those in Ubuntu OS and while installing I'm facing the issues mentioned above..

 

PS : I'm doing so, to program a custom board KM34 via this onboard debugger using LPC4322 MCU

0 Kudos
Reply

2,098 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

I create new case 00572365 to our RT engineer, she will give update to you then you will receive the email.