How to install OpenGL in Yocto to resolve "No GL implementation is available" error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to install OpenGL in Yocto to resolve "No GL implementation is available" error

5,581 Views
hareendran-tl
Contributor II

I'm encountering an issue when running an application on my Yocto-based system, and I'm getting the error message: "Failed to start Flutter renderer: No GL implementation is available." Additionally, when I check the existence of the 'gtk+-3.0' package using `pkg-config`, it shows that the 'gl' package is not found in the search path and suggests adding the directory containing 'gl.pc' to the `PKG_CONFIG_PATH` environment variable.


root@apalis-imx8-07013820:/usr/lib/pkgconfig# pkg-config --exists --print-errors 'gtk+-3.0'
Package gl was not found in the pkg-config search path.
Perhaps you should add the directory containing `gl.pc'
to the PKG_CONFIG_PATH environment variable
Package 'gl', required by 'epoxy', not found

I have already added the 'mesa' package to my local.conf, but it seems that 'gl.pc' is not present in the '/usr/lib/pkgconfig' directory. When I open the 'epoxy.pc' file, it shows the following content:


prefix=/usr
libdir=${prefix}/lib
includedir=${prefix}/include

epoxy_has_glx=1
epoxy_has_egl=1
epoxy_has_wgl=0

Name: epoxy
Description: GL dispatch library
Version: 1.5.10
Requires.private: x11, egl, gl egl
Libs: -L${libdir} -lepoxy
Libs.private: -ldl
Cflags: -I${includedir}

I would appreciate any guidance on how to properly install OpenGL or resolve the "No GL implementation is available" error in Yocto. Additionally, I'd like to know how to ensure that 'gl.pc' is available in the '/usr/lib/pkgconfig' directory. Thank you for your help!

Tried to install OpenGL in Yocto. Expected success, got "No GL implementation" error.

Tags (3)
0 Kudos
Reply
3 Replies

5,530 Views
hareendran-tl
Contributor II

Hi @Manuel_Salas ,

I'm using Ubuntu 20.04 as my host system for Yocto build and i want to compile Linux version 5.15.129.

When I added libgl-mesa-dev package to the yocto and the gl.pc file created under the pkgconfig directory and the error when running the pkg-config --exists --print-errors 'gtk+-3.0' command was gone.

But the following error when running the application still persist.
WARNING **: 06:27:15.221: Failed to start Flutter renderer: No GL implementation is available

0 Kudos
Reply

5,532 Views
hareendran-tl
Contributor II

Hi @Manuel_Salas ,

I'm using Ubuntu 20.04 as my host system for the Yocto build.
I want to compile Linux 5.15.129.

And when I added libgl-mesa-dev package to the yocto and the gl.pc file created under the pkgconfig directory and the error when running the pkg-config --exists --print-errors 'gtk+-3.0' command was gone.

But the following error when running the application still persist.
WARNING **: 06:27:15.221: Failed to start Flutter renderer: No GL implementation is available

0 Kudos
Reply

5,561 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @hareendran-tl ,

 

Could you please share more details about of the environment?

For example, what Ubuntu version are you using in your host, what Linux version you want to compile, etc.

 

Also, you can try:

$ sudo apt install libgl1-mesa-dev

$ export PKG_CONFIG_PATH=/usr/lib/x86_64-linux-gnu/pkgconfig

$ export DISPLAY=$(cat /etc/resolv.conf | grep nameserver | awk '{print $2}'):0

 

 

Best regards!

0 Kudos
Reply