Hello I'm working with i.MX53QSB (loco board) with Linux. I'm successfully using LTIB.
I would like to use Eclipse for writing application, but I have some problems.
I have configured the Eclipse like it is described in the Application note "Developing an Application for the i.MX Devices on the Linux Platform" here: http://cache.freescale.com/files/dsp/doc/app_note/AN3870.pdf
When I include some standard file like #include <linux/input.h> there is no problem. But I would like to include another files for example /<LTIB_PATH>/rpm/BUILD/linux/include/linux/pmic_external.h in this case there are compile errors.
Maybe the problem is that #include <linux/input.h> includes /usr/include/linux/input.h not /<LTIB_PATH>/rpm/BUILD/linux/include/linux/input.h
There are probably missing some compiler parametters, but I'm not able to solve it.
Please, could anyone help?
Karel
Message was edited by: Karel Havlovic