How to improve GPIO frequency

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to improve GPIO frequency

1,843件の閲覧回数
linhaiboyy
Contributor II

I am working on Mx6q,I want to use GPIO Simulation time sequence, but the frequency maximum reach  500K.How can I configure GPIO work faster ?

ラベル(1)
0 件の賞賛
返信
1 返信

1,613件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

there is no simple way as toggle speed depends on internal

delays. Some customers succeeded enabling MMU, L2 cache,

and set the mmu entry that cover the GPIO_DR address of Device type.

It may be useful to check

imx6 running slow 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信