How to improve GPIO frequency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to improve GPIO frequency

1,889 Views
linhaiboyy
Contributor II

I am working on Mx6q,I want to use GPIO Simulation time sequence, but the frequency maximum reach  500K.How can I configure GPIO work faster ?

Labels (1)
0 Kudos
Reply
1 Reply

1,659 Views
igorpadykov
NXP Employee
NXP Employee

Hi

there is no simple way as toggle speed depends on internal

delays. Some customers succeeded enabling MMU, L2 cache,

and set the mmu entry that cover the GPIO_DR address of Device type.

It may be useful to check

imx6 running slow 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply