It seems that the OpenCL support on i.MX6Q (at least with 3.10.17 BSP) doesn't have the built-in atomic functions such as atomic_inc() etc.
Are there ways to implement that function on i.MX6Q?
 
					
				
		
 jamesbone
		
			jamesbone
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello Yanfeng,
The atomic functions are currently disable from OpenCL compiler, we are working to have another version of the driver of the GPU to support this functions in the near future. I do not have a date to provide but this are part of the pipeline.
Hello jamesbone,
I just have met the same problem when i tried to build an application to achieve hough line transform with opencl, but "atomic_add/inc" was not supported, is there recent update support this function?
Thanks for the updates. I will then use OpenCL for cases where such function is not needed with current version. :smileyhappy:
I just have met the same problem when i tried to build an application to achieve hough line transform with opencl, but "atomic_add/inc" was not supported, is there recent update support this function?