How to implement DMA controller in PCIe root complex(RC) mode?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to implement DMA controller in PCIe root complex(RC) mode?

3,116件の閲覧回数
mimi05633
Contributor III

Hi NXP team,

In the IMX8MDQLQ reference manual, I can see PCIe has an embedded DMA.
How to implement DMA controller in PCIe root complex(RC) mode? And does any kernel config need to enable?

Topology: IMX8MQ(RC) ---(mini-pcie)--- FPGA(EP)

My harware:
- IMX8MQ customize board (software: LF_L5.4.3_1.0.0)

I appreciate if someone can help me to solve it.

Thank you for any help.
Minying

ラベル(1)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

3,114件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信

3,110件の閲覧回数
mimi05633
Contributor III

Hi Igor,
Thank you for your reply.
In the pci_imx6.c, there is a self io test by dma in EP mode. Can it also be used in RC mode?
If yes, can the self io test be used after PCIe links up? Is there a need to do other initial setups before the self io test?

Best regards,
minying

0 件の賞賛
返信