How to implement DMA controller in PCIe root complex(RC) mode?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to implement DMA controller in PCIe root complex(RC) mode?

3,096 次查看
mimi05633
Contributor III

Hi NXP team,

In the IMX8MDQLQ reference manual, I can see PCIe has an embedded DMA.
How to implement DMA controller in PCIe root complex(RC) mode? And does any kernel config need to enable?

Topology: IMX8MQ(RC) ---(mini-pcie)--- FPGA(EP)

My harware:
- IMX8MQ customize board (software: LF_L5.4.3_1.0.0)

I appreciate if someone can help me to solve it.

Thank you for any help.
Minying

标签 (1)
标记 (2)
0 项奖励
回复
2 回复数

3,094 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复

3,090 次查看
mimi05633
Contributor III

Hi Igor,
Thank you for your reply.
In the pci_imx6.c, there is a self io test by dma in EP mode. Can it also be used in RC mode?
If yes, can the self io test be used after PCIe links up? Is there a need to do other initial setups before the self io test?

Best regards,
minying

0 项奖励
回复