How to identify display on imx8qxp

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to identify display on imx8qxp

1,619 次查看
jordonwu
Contributor III

As imx8qxp can driver more displays(DSI0, DSI1 and LCDIF),  How to identify display in application while all these display drived ? thanks.

our test environment is L4.14.98_2.3.0_images_MX8QXPMEK(rootfs is fsl-image-validation-imx-imx8qxpc0mek.tar.bz2

  ), thanks.

0 项奖励
回复
3 回复数

1,554 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

These DTS files affect the behavior of the displays connected to the mini-SAS connectors, which expand your
multimedia experience in combination with the range of daughter cards available for the i.MX8QXP MEK.

How to set you can see

Changing DTS files on Linux.PNG

https://www.nxp.com/webapp/Download?colCode=AN12189 

https://www.nxp.com/webapp/Download?colCode=AN12188 

https://www.nxp.com/webapp/Download?colCode=AN12187 

You can refer to these documents.

Have a nice day

Best Regards

Rita

0 项奖励
回复

1,554 次查看
jordonwu
Contributor III

Hi Rita Wang,

Thanks for your feedback. 

Sorry, maybe I'm not statement my question clearly. Now we have success drive two display (one is via DSI0 and another is via DSI1)  on imx8qxp board. my question is:

In user space, how the application switch the content to different display panel?  For example, we call DSI0 lvds as display0 and DSI1 lvds as display1, in user space application, how to decide the application's contest displayed on display0 or display1? 

thanks.

0 项奖励
回复

1,554 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

https://community.nxp.com/docs/DOC-342059 this may do help for you.

0 项奖励
回复