How to identify display on imx8qxp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to identify display on imx8qxp

1,628 Views
jordonwu
Contributor III

As imx8qxp can driver more displays(DSI0, DSI1 and LCDIF),  How to identify display in application while all these display drived ? thanks.

our test environment is L4.14.98_2.3.0_images_MX8QXPMEK(rootfs is fsl-image-validation-imx-imx8qxpc0mek.tar.bz2

  ), thanks.

0 Kudos
Reply
3 Replies

1,563 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

These DTS files affect the behavior of the displays connected to the mini-SAS connectors, which expand your
multimedia experience in combination with the range of daughter cards available for the i.MX8QXP MEK.

How to set you can see

Changing DTS files on Linux.PNG

https://www.nxp.com/webapp/Download?colCode=AN12189 

https://www.nxp.com/webapp/Download?colCode=AN12188 

https://www.nxp.com/webapp/Download?colCode=AN12187 

You can refer to these documents.

Have a nice day

Best Regards

Rita

0 Kudos
Reply

1,563 Views
jordonwu
Contributor III

Hi Rita Wang,

Thanks for your feedback. 

Sorry, maybe I'm not statement my question clearly. Now we have success drive two display (one is via DSI0 and another is via DSI1)  on imx8qxp board. my question is:

In user space, how the application switch the content to different display panel?  For example, we call DSI0 lvds as display0 and DSI1 lvds as display1, in user space application, how to decide the application's contest displayed on display0 or display1? 

thanks.

0 Kudos
Reply

1,563 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

https://community.nxp.com/docs/DOC-342059 this may do help for you.

0 Kudos
Reply