Thanks for that Claudiu , but it didn't work for me. Actually I have selected DISTRO as x11 and build the image as fsl-image-qt5 .
If do bitbake fsl-image-qt5 -c populate_sdk , I didn't get qmake in sdk which is required for cross compiling.
I tried with bitbake meta-toolchain-qt5 and got qmake but while cross compiling I was unable to generate output .
I used qt creator 5.8.0 and set the cross compiler toolkit properly , but it gave following errors:
g++ -o QtExample main.o exqamplewidget.o moc_exqamplewidget.o -lQt5Widgets -lQt5Gui -lQt5Core -lGLESv2 -lpthread
/usr/bin/ld: cannot find -lQt5Widgets
/usr/bin/ld: cannot find -lQt5Gui
/usr/bin/ld: cannot find -lQt5Core
/usr/bin/ld: cannot find -lGLESv2
collect2: error: ld returned 1 exit status
make: *** [QtExample] Error 1
12:47:06: The process "/usr/bin/make" exited with code 2.
Error while building/deploying project QtExample (kit: iMX-6)
The kit iMX-6 has configuration issues which might be the root cause for this problem.
When executing step "Make"
12:47:06: Elapsed time: 00:00.
Please give the solution .
Thanks ,
Abhirup Mitra