How to get mux 32bit work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to get mux 32bit work

1,805 Views
jasonpan
Contributor I

I am using i.mx6 solo processor connected to FPGA through EMI bus. I want to read and write 32bit data from the FPGA. I use Mux mode with DSZ=011( 26bit address:16bit AD+EIM data(0~9), 32bit data:16bit AD+EIM data(0~15),But CPU reset after writing 32 bit data to FPGA. does someone found this issues?

pastedImage_1.png

0 Kudos
Reply
2 Replies

1,720 Views
jasonpan
Contributor I

Hi Yuri,

thanks for your comments,

our current configure as below:(It work at mux 16bit mode, but 32bit will reset at second write process), would you help check if something we missed? thanks

regval = val | 0x7<<28 | (0x3 << 16)| 0x4<<8 | 0x7<<3 | 0x3<<1 | 1<<2 | 1<<23;

writel( regval, WEIM_BASE_ADDR );

regval= 0x1;

writel(regval,WEIM_BASE_ADDR+0x4);

//write timimg

//WSC=6, ADVA=0, ADVN=1, ADH=1

regval = 0x6<<24 | 0x1<<18;

writel(regval, WEIM_BASE_ADDR + 0x10);

//WSC=7, RADVN=1, ADH=1, OEA=0

regval = 0x7<<24 | 0x1<<16;

writel(regval, WEIM_BASE_ADDR + 0x8);

iomux_v3_cfg_t eimfpga_da_pads[] = {

              //EIM_AD[15:0]

              MX6_PAD_EIM_DA0__WEIM_WEIM_DA_A_0   | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_EIM_DA1__WEIM_WEIM_DA_A_1   | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_EIM_DA2__WEIM_WEIM_DA_A_2   | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_EIM_DA3__WEIM_WEIM_DA_A_3   | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_EIM_DA4__WEIM_WEIM_DA_A_4   | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_EIM_DA5__WEIM_WEIM_DA_A_5   | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_EIM_DA7__WEIM_WEIM_DA_A_7   | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_EIM_DA8__WEIM_WEIM_DA_A_8   | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_EIM_DA9__WEIM_WEIM_DA_A_9   | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_EIM_DA10__WEIM_WEIM_DA_A_10 | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_EIM_DA11__WEIM_WEIM_DA_A_11 | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_EIM_DA12__WEIM_WEIM_DA_A_12 | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_EIM_DA13__WEIM_WEIM_DA_A_13 | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_EIM_DA14__WEIM_WEIM_DA_A_14 | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_EIM_DA15__WEIM_WEIM_DA_A_15 | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              //EIM_A_D[25:16]         

              MX6_PAD_CSI0_DATA_EN__WEIM_WEIM_D_0 | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_CSI0_VSYNC__WEIM_WEIM_D_1      | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),          

              MX6_PAD_CSI0_DAT4__WEIM_WEIM_D_2        | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_CSI0_DAT5__WEIM_WEIM_D_3        | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_CSI0_DAT6__WEIM_WEIM_D_4        | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_CSI0_DAT7__WEIM_WEIM_D_5        | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_CSI0_DAT8__WEIM_WEIM_D_6        | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_CSI0_DAT9__WEIM_WEIM_D_7        | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_CSI0_DAT12__WEIM_WEIM_D_8      | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_CSI0_DAT13__WEIM_WEIM_D_9      | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              //EIM_DATA[31:26]

              MX6_PAD_CSI0_DAT14__WEIM_WEIM_D_10    | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_CSI0_DAT15__WEIM_WEIM_D_11    | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_CSI0_DAT16__WEIM_WEIM_D_12    | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_CSI0_DAT17__WEIM_WEIM_D_13    | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_CSI0_DAT18__WEIM_WEIM_D_14    | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_CSI0_DAT19__WEIM_WEIM_D_15    | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

             

   MX6_PAD_EIM_LBA__WEIM_WEIM_LBA | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_EIM_OE__WEIM_WEIM_OE   | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_EIM_RW__WEIM_WEIM_RW   | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_EIM_CS0__WEIM_WEIM_CS_0 | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),

              MX6_PAD_EIM_CS1__WEIM_WEIM_CS_1 | MUX_PAD_CTRL(WEIM_NOR_PAD_CTRL),          

};

 

Br,

Jason

0 Kudos
Reply

1,720 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please check if EIM clock is not gated in CCM Clock Gating Register (CCM_CCGR6).

 Also,  section 22.6 (Initialization Information) of i.MX6 S/DL RM (IMX6SDLRM,
Rev. 2, 04/2015) contains examples of EIM initialization.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply