How to get gcc source code for i.MX6 Linux BSP.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to get gcc source code for i.MX6 Linux BSP.

Jump to solution
6,084 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6 Linux BSP (L3.0.35_4.1.0 & L3.10.17_1.0.2-ga).

I'm looking for the source code of GCC compiler.

I found the source code for i.MX51 in the following URL.

i.MX51 Evaluation Kit|Freescale

Is GCC compiler source code for i.MX6 opened same as the one for i.MX51 even though I cannot found it on i.MX6 web page?

Or should I download it from Linaro web site?

Best Regards,

Satoshi Shimoda

Tags (1)
0 Kudos
Reply
1 Solution
5,406 Views
igorpadykov
NXP Employee
NXP Employee

!!Hi Satoshi

please look at attached documents for compilers selection.

Source codes can be found on gcc web site

GCC, the GNU Compiler Collection- GNU Project - Free Software Foundation (FSF)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
5,407 Views
igorpadykov
NXP Employee
NXP Employee

!!Hi Satoshi

please look at attached documents for compilers selection.

Source codes can be found on gcc web site

GCC, the GNU Compiler Collection- GNU Project - Free Software Foundation (FSF)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply