How to get data use csi0 parallel port ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to get data use csi0 parallel port ?

809 次查看
hanseunglee
Contributor III

------------------------------------------------------

Kernel : 3.0.35

Board : i.mx6dl-sabresd

OS : ubuntu 12.04

------------------------------------------------------

Hello , everyone!

Test the data transfer use csi0 port.

I send data to i.mx6 board .

we want to  data transform is below fig.

 

146508_146508.pngpastedImage_1.png

use BT656

 

146507_146507.jpgbt656 interface.jpg

result data file.

 

146509_146509.jpgresult_data.jpg

 

----------------------------------------------------------------------------------------------------------------------------------

use test program : mxc_v4l2_capture.c (device driver) file and mxc_v4l2.capture.c(app) .

size 1024 * 768

 

----------------------------------------------------------------------------------------------------------------------------------

i want to get data like that 0 1 2 3 4 5 .... 255 .... but result of test is not good.

 

when i get data ,result is 0 0 0 1 1 1 2 2 3  3 4 4 ... 255  ..

 

Why am i get wrong data...?  please reply your opinion..

 

wrong data file is attach this page.

Original Attachment has been moved to: cbcr_sep1.yuyv.zip

标签 (1)
0 项奖励
回复
1 回复

719 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Hanseung

for BT656 format mxc_v4l2_tvin should be used

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复