How to get clock on CCM_CLKO1 for imx6q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to get clock on CCM_CLKO1 for imx6q

1,830 次查看
vasusriram
Contributor II

Hi,

I am working on imx6q board. I am trying to get clock on CCM_CLKO1 (D16 Pin) 24MHz or 12MHz.

while ov5640_mipi is loading i am getting clock for 1 sec later it is disabled. Some times it is showing as 24MHz on scope and some times <10Hz.

How to get clock continuosly on D16 or C22 pins.

I have attached my dtsi file please help me as soon as possible. And i am new to working on clock.

imx6q 5.0.2 android and linux 3.10 kernel version.

Thanks add Regards,

R S S Vasu Naidu.

Mail ID : vasu.r@affluencesystems.com.

标记 (1)
0 项奖励
回复
1 回复

1,516 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vasu

one can refer to

IMX6 27MHz on CSI_MCLK 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复