How to get a sensor list of MCIMX8M-EVK board in Android Sensor Framework?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to get a sensor list of MCIMX8M-EVK board in Android Sensor Framework?

1,875 Views
sky1
Contributor I

Hi,

I have 2 imx boards, MCIMX6Q-SDB and MCIMX8M-EVK.

I developed Android App.(SensorList.apk) to get a sensor list from these boards.

I can get the list from MCIMX6Q-SDB board, but NOT MCIMX8M-EVK.board.

1. MCIMX6Q-SDB

My "SensorList" App. shows following information.

-----------------------------------------------------------------------------------------------------

Number of Sensors: 5

Freescale 3-axis Accelerometer

Type: TYPE_ACCELEROMETER
Vendor: Freescale Semiconductor Inc.
Version: 1

Resolution: 5.985504E-4

MaxumumRange: 1500.0
Power: 0.3

...

-----------------------------------------------------------------------------------------------------

This information is same as that of sSensorList structure in sensors.cpp file.

This file is in $(MY_ANDROID)/vendor/nxp-opensource/imx/libsensors directory.

static const struct sensor_t sSensorList[] = {
{
.name = "Freescale 3-axis Accelerometer",
.vendor = "Freescale Semiconductor Inc.",
.version= 1,
.handle = SENSORS_ACCELERATION_HANDLE,
.type = SENSOR_TYPE_ACCELEROMETER,
.maxRange = RANGE_A,
.resolution = CONVERT_A,
.power = 0.30f,
.minDelay = 2500,
.fifoReservedEventCount = 0,
.fifoMaxEventCount = 32,
.stringType = SENSOR_STRING_TYPE_ACCELEROMETER,
.requiredPermission = 0,
.maxDelay = 640000,
.flags = SENSOR_FLAG_CONTINUOUS_MODE,
.reserved = {}
},

...

...

...

2. MCIMX8M-EVK

My "SensorList" App. shows no sensor information as follows.

-----------------------------------------------------------------------------------------------------

Number of Sensors: 0

-----------------------------------------------------------------------------------------------------

But sensors.cpp in

$(MY_ANDROID)/vendor/nxp-opensource/imx/libsensors_sensorhub directory

has following sensor information.

static const struct sensor_t sSensorList[] = {
{
.name = "Freescale Sensor Hub Accelerometer",
.vendor = "Freescale Semiconductor Inc.",
.version= 1,
.handle = SENSORS_ACCELERATION_HANDLE,
.type = SENSOR_TYPE_ACCELEROMETER,
.maxRange = RANGE_A,
.resolution = CONVERT_A,
.power = 0.30f,
.minDelay = 2500,
.fifoReservedEventCount = 0,
.fifoMaxEventCount = 0,
.stringType = SENSOR_STRING_TYPE_ACCELEROMETER,
.requiredPermission = 0,
.maxDelay = 640000,
.flags = SENSOR_FLAG_CONTINUOUS_MODE,
.reserved = {}
},

...

...

...

How can I get the sensor list (in sensors.cpp) in MCIMX8M-EVK development environment?

MCIMX6Q-SDB board has real H/W sensors, but MCIMX8M-EVK board does not.

I think that the absence of real sensors has no effect on getting the sensor list.

Is it correct?

Pleas help me to fix this problem.

Thanks in advance.

0 Kudos
Reply
2 Replies

1,660 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi james,

    There is no sensor supported on i.MX8M-EVK,  It means that there is no any sensors hardware related to libsensor.  So you couldn't get corresponding list.

Have a nice day!

TIC weidong sun

0 Kudos
Reply

1,660 Views
sky1
Contributor I

Hi weidong,

Thanks for your response.

I think that my question was not clear.

Anyway, one more question.

I wrote a simple linux kernel driver which simply emulate some accelerometer functions.

(such as 'enable', 'power', 'report input event', ...)

And linux kernel log shows this driver is successfully probed as following.

-----------------------------------------------------------------------------------------------------------------

[ 2.396065] input: FreescaleGyroscope as /devices/virtual/input/input0
[ 2.402876] fxas2100x device driver probe successfully

-----------------------------------------------------------------------------------------------------------------

device node created

crw------- 1 root root 10,  61 1970-01-01 00:00 /dev/FreescaleGyroscope

also sysfs is created

/sys/class/misc/FreescaleGyroscope

/sys/class/misc/FreescaleGyroscope/uevent   shows

MAJOR=10

MINOR=61

DEVNAME=FreescaleGyroscope

In this situation,

How can I get a list of the sensors in Android Sensor Framework?

(My SensorList App. just called the 'getSensorList' functions)

I'm not experienced in such things,

Please give me some tips for registering new  sensors into given iMX8 board which has no sensors.

Thanks very much.

0 Kudos
Reply