How to get U-Boot image information in "U-Boot 2016.03 " version ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to get U-Boot image information in "U-Boot 2016.03 " version ?

972 次查看
jones_chang
Contributor II

Hi Yuri,

Thanks for your reply.

I will focus on AN4581.pdf about signing boot image

Another question:

How to get U-Boot image information in "U-Boot 2016.03 " version ?

the information is like following

-----following is AN4581.pfd content--------------------

E.2. From mkimage tool log
Since U-Boot v2017.01 a build log containing the data above is available after building U-Boot:
$ cat u-boot-dtb.imx.log
Image Type: Freescale IMX Boot Image
Image Ver: 2 (i.MX53/6/7 compatible)
Mode: DCD
Data Size: 602112 Bytes = 588.00 KiB = 0.57 MiB
Load Address: 877ff420
Entry Point: 87800000
HAB Blocks: 877ff400 00000000 0008ec00
DCD Blocks: 00910000 0000002c 000001c4

0 项奖励
回复
1 回复

881 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

  Use section E.1 (Dumping U-boot binary) of the AN4581.

 

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 项奖励
回复