How to get Maximum Supply Currents

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to get Maximum Supply Currents

ソリューションへジャンプ
2,117件の閲覧回数
ko-hey
Senior Contributor II

Hi all

As for the "Table 14. Maximum Supply Currents" in IMX6SXCEC.

It's not mentioned about how to get a value.

I found a calculation formula for i.MX6Q from following thread in i.MX community.

About max supply current in i.MX6Q.

The formula is as follow.

--------------------------------------------------

General equation for estimated, maximum power consumption of an IO power supply:

Imax = N x C x V x (0.5 x F)

Where:

N—Number of IO pins supplied by the power line

C—Equivalent external capacitive load

V—IO voltage

(0.5 xF)—Data change rate. Up to 0.5 of the clock rate (F)

In this equation, Imax is in Amps, C in Farads, V in Volts, and F in Hertz.

--------------------------------------------------

Is the formula appropriate to i.MX6SoloX ?

Ko-hey

ラベル(3)
0 件の賞賛
返信
1 解決策
1,952件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

you are right: this formula is applicable to i.MX6SX too.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,953件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

you are right: this formula is applicable to i.MX6SX too.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,952件の閲覧回数
ko-hey
Senior Contributor II

Hi Igor

Thank you for quick reply.

I understand.

Ko-hey

0 件の賞賛
返信